i.MX6 sole(MCIMX6S7CVM08AC) which dtb should I use

cancel
Showing results for 
Search instead for 
Did you mean: 

i.MX6 sole(MCIMX6S7CVM08AC) which dtb should I use

304 Views
kwyang
Contributor I

Hello,

I have a question about choosing dtb files.

I'm using i.MX Solo (MCIMX6S7CVM08AC).

When I connect USB, it shows PID 61 which is MX6D. I thought that is should  PID 63 which is MX6SL

but since there, I'm applying all dtb and config files to mx6dl_sabresd files because it shows MX6D

Am I doing right? using mx6dl? or should I use mx6sl_evk files..?

which dtb or config files should I choose?

Labels (5)
0 Kudos
1 Reply

245 Views
b45499
NXP TechSupport
NXP TechSupport

The i.MX6Solo  you can refer to the i.MX6DL design, so you can use the i.mx6dl.

0 Kudos