Hello,
I have a question about choosing dtb files.
I'm using i.MX Solo (MCIMX6S7CVM08AC).
When I connect USB, it shows PID 61 which is MX6D. I thought that is should PID 63 which is MX6SL
but since there, I'm applying all dtb and config files to mx6dl_sabresd files because it shows MX6D
Am I doing right? using mx6dl? or should I use mx6sl_evk files..?
which dtb or config files should I choose?
The i.MX6Solo you can refer to the i.MX6DL design, so you can use the i.mx6dl.