i.MX6 shutdown with temperature monitor question

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX6 shutdown with temperature monitor question

1,862 Views
m_c
Senior Contributor I

<linux-2.6-imx.git - Freescale i.MX Linux Tree >

1. Did (TEMP_CRITICAL, TEMP_HOT, TEMP_ACTIVE) need to calibration on customer i.MX6 board?

2. Did i.MX6 has hardware protection mechanism (ex: shutdown processor) when operating temperature over specification if software temperature monitor disabled or fail?

Labels (1)
0 Kudos
Reply
1 Reply

1,301 Views
Yuri
NXP Employee
NXP Employee

Hello,

 The i.MX6 does not support hardware thermal shutdown mechanism.
Please use app note " i.MX 6 Temperature Sensor Module " and Chapter 25 (Thermal Driver) of
"i.MX_Linux_Reference_Manual.pdf" regarding thermal protection approach for i.MX6.

http://www.nxp.com/assets/documents/data/en/application-notes/AN5215.pdf 

http://www.nxp.com/webapp/Download?colCode=L4.1.15_2.0.0-LINUX-DOCS 

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply