i.MX6 sata HDD cannot find device node on Kernel 4.9.11

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

i.MX6 sata HDD cannot find device node on Kernel 4.9.11

跳至解决方案
1,715 次查看
mayqueen
Contributor IV

Hello all:

I trying the latest SDK - kernel 4.9.11 on i.MX6 platform, but when I test SATA interface, I can't see any /dev/sdx relative device node, but kernel message is works as following:

ata1: SATA link up 3.0 Gbps (SStatus 123 SControl 300)
ata1.00: ATA-9: TS128GSSD340, SVN423b, max UDMA/100
ata1.00: 250069680 sectors, multi 16: LBA48 NCQ (depth 31/32)
ata1.00: configured for UDMA/100

What's wrong with SATA function?? what can I do to fix it? It's normal working on 4.1.15, thanks!

标签 (3)
标记 (2)
0 项奖励
回复
1 解答
1,555 次查看
mayqueen
Contributor IV

Sorry, it's defconfig issue if copy from 4.1.15, it works using 4.9.11 defconfig.

在原帖中查看解决方案

0 项奖励
回复
2 回复数
1,556 次查看
mayqueen
Contributor IV

Sorry, it's defconfig issue if copy from 4.1.15, it works using 4.9.11 defconfig.

0 项奖励
回复
1,555 次查看
CarlosCasillas
NXP Employee
NXP Employee

Hi May,

Thanks for sharing your solution with the Community.

Best regards!

/Carlos

0 项奖励
回复