i.MX6 reset question

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX6 reset question

856件の閲覧回数
jamesdavis
Contributor III
  1. Will ARM core-reset reset AXI bus?

  1. Is IPU reset necessary if ARM core is reset?
ラベル(1)
0 件の賞賛
返信
1 返信

739件の閲覧回数
Yuri
NXP Employee
NXP Employee

  Please refer to Chapter 60 [System Reset Controller (SRC)] of the i.MX6
DQ Reference Manual about reset signals of the i.MX6.

In particular Figure 60-5 (SRC inputs and outputs) shows input reset events.

All of them reset both ARM (including buses) and IPU.


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信