i.MX6 pad drive strength setting

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX6 pad drive strength setting

Jump to solution
1,280 Views
torus1000
Contributor V

Hi,

Pad drive strength recommended 8mA on p2571 in i.MX6DQ RM rev2.0.

Which DSE setting is correct to drive 8mA @3.3V for SD4_CMD pad?

DSE=
001 150 Ohm @ 3.3V, 260 Ohm @ 1.8V
010 75 Ohm @ 3.3V, 130 Ohm @ 1.8V
011 50 Ohm @ 3.3V, 90 Ohm @ 1.8V
100 37 Ohm @ 3.3V, 60 Ohm @ 1.8V
101 30 Ohm @ 3.3V, 50 Ohm @ 1.8V
110 25 Ohm @ 3.3V, 40 Ohm @ 1.8V
111 20 Ohm @ 3.3V, 33 Ohm @ 1.8V

On th other hand, an IBIS model (gpiohv_ds001_sr000_mio:GPIO,3.3V,DSE=001)
shows Ioh@3.3=10.7mA.

Is it OK to set DSE=001 for 8mA current?

mx6q_ibis.png

Thanks,

Labels (1)
Tags (2)
1 Solution
789 Views
igorpadykov
NXP Employee
NXP Employee

Hi torus1000

I think you are right,  DSE=001 for 8mA current

is proper selection.

Best regards

igor
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
790 Views
igorpadykov
NXP Employee
NXP Employee

Hi torus1000

I think you are right,  DSE=001 for 8mA current

is proper selection.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos