使用官方提供的M6.0的从uboot到kernel保持的patch,整个过程可以loading到kernel,但是在kernel和uboot衔接阶段出现闪屏,并没有平稳过渡,同时从kernel的logo过渡到动态logo阶段,也会有闪屏。
之前有联系过nxp的FAE,但是回复使用该补丁不会存在该问题,我这边也多次核对过patch,甚至连JB4.2.2里的“0003-Skip-lvds-re-initialization-for-logo-keep.patch”看过一遍,在现有的内核里都有确实已经修改了。
问题困扰了几天了,还请帮忙给个思路,谢谢~
You can refer to https://community.nxp.com/docs/DOC-98109 .