i.MX6 is not booting up after secure boot!!!

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX6 is not booting up after secure boot!!!

1,918 Views
ericg
Contributor II

OTPMK seemed already burned as shown below:

=> md 0x020cc014 1

020cc014: 80009b00

We've already burned SRK fuses and get the HAB working in open mode. However, after executing the following to close the config to enable secure boot, device is not booting anymore.

=> fuse prog 0 6 0x02

Programming bank 0 word 0x00000006 to 0x00000002...

What could be the issue, please help! Thanks.

Labels (1)
0 Kudos
Reply
4 Replies

1,735 Views
manliu
Contributor I

I'm facing exactly the same problem. Please let me known if you have worked out the issue.

Thanks

Best Regards

0 Kudos
Reply

1,735 Views
ericg
Contributor II

What about the linker script in secure boot mode? Could it be something to with linker script? If u-boot boots up in open mode then can we say that linker script is correct?

0 Kudos
Reply

1,735 Views
manliu
Contributor I

I'm not sure. There was once something wrong with the linker script, but it led to some HAB events. After i changed something in the linker script, the HAB events went away.

0 Kudos
Reply

1,735 Views
gusarambula
NXP TechSupport
NXP TechSupport

Hello Ericg,

You may find the Application Note 4581 useful (link below). Additional information regarding HAB can be found on the i.MX6 Security Reference Manual, which is moderated and this require an NDA. If you need further assistance please open a Case since these matters cannot be handled on the public communities.

http://cache.nxp.com/files/32bit/doc/app_note/AN4581.pdf

Regards,

0 Kudos
Reply