[i.MX6 history] Does anybody know what this Freescale board is?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

[i.MX6 history] Does anybody know what this Freescale board is?

Jump to solution
656 Views
DiegoFSL
Contributor III

Hi i.MX Community,

I'd like to kindly as if anybody knows what this board listed here is:

NXP / FREESCALE i.MX6Q: i.MX 6Quad - SABRE Board for Smart Devices 

It is advertised in the title as a "i.MX6Quad SABRE SD" but it is very different to the regular SABRE SD:

  1. PCB is red instead of green
  2. production year is 2011 instead of 2012
  3. layout is very different
  4. I can't seem to spot the i.MX6Q SOC on the PCB, the one in the center is a Micron chip
  5. the board is labelled "MX6QCPUPOP" instead of "MCIMX6Q-SDB"
  6. serial number is very low, it's "S/N 0006"

Is it some kind of SABRE SD prototype or something else?

Any kind of information or help will be really appreciated.

Thanks.

MX6QCPUPOP board

Labels (1)
1 Solution
503 Views
gusarambula
NXP TechSupport
NXP TechSupport

From the board number it is the i.MX6 LPDDR2 PoP CPU board, but it is a prototype. (Given by the X revision). Current revision of the board is B1.

View solution in original post

2 Replies
503 Views
mooreaa
Contributor II

Based on the POP memory from Micron its likely that its the POP version of the i.MX6. 

http://www.nxp.com/assets/documents/data/en/data-sheets/IMX6DQCPOPEC.pdf 

Haven't seen this board but going by the S/N 0006 it seems like a pretty early rev board maybe.

504 Views
gusarambula
NXP TechSupport
NXP TechSupport

From the board number it is the i.MX6 LPDDR2 PoP CPU board, but it is a prototype. (Given by the X revision). Current revision of the board is B1.