i.MX6 eCSPI Write/Read Timing Understanding

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

i.MX6 eCSPI Write/Read Timing Understanding

跳至解决方案
1,436 次查看
chris_lambrecht
Contributor III

In looking at the Electrical Characteristics for the i.MX6 ULL processor (IMX6ULLCED PDF), Figure 35 and Table 47 indicate that there is a SPI Write timing of 15ns while there is a SPI Read Timing of 43ns (CS1) in Master Mode.

I read this to mean that the MISO data will not be registered correctly by the i.MX6 ULL processor if the i.MX6 is generating a SPI SCLK at a frequency greater than 23MHz (43ns). Therefore, if the i.MX6 wants to be able to register MISO data correctly, it must always run with a SPI clock slower than 43ns, or change between a faster clock when it doesn't care about the MISO data and a slower clock, when it does care to receive valid data.

Is this a correct understanding of these two timing parameters?

Thanks,

Chris

标签 (1)
0 项奖励
回复
1 解答
1,430 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Chris

 

yes your understanding is correct.

 

Best regards
igor

在原帖中查看解决方案

0 项奖励
回复
2 回复数
1,425 次查看
chris_lambrecht
Contributor III

Thanks!!

0 项奖励
回复
1,431 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Chris

 

yes your understanding is correct.

 

Best regards
igor

0 项奖励
回复