i.MX6 duallite-60FPS

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX6 duallite-60FPS

Jump to solution
1,137 Views
muthurajm
Contributor III

Dear all,

we are using IMX6 Dual processor to run a Full HD Animated image in our TFT.

Now the image Frame rate 30 FPS.

Does our processor have the capability to run the same in 60 FPS?

NOTE:

1. In the Datasheet it has mentioned without "Multimedia Framework" the The video can be recorded and the same can be playbacked at 60 FPS.

Kinldy HELP:)

Regards,

Muthuraj M

+919003281838

Labels (2)
Tags (1)
0 Kudos
1 Solution
860 Views
igorpadykov
NXP Employee
NXP Employee

Hi Muthuraj

typical value is 30fps as shown on presentation p.21

A Deep Dive into Image Processing for i.MX 6 Series Applications Processors

p.118 shows 60fps use case.

Performance depends om use case, since some IPU submodules are limited to 1920x1080 @ 30 fps,

sect.38.1.2.1.5.3 Image Converter (IC) IMX6SDLRM

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
3 Replies
860 Views
muthurajm
Contributor III

Thanks a lot Igor:)

0 Kudos
861 Views
igorpadykov
NXP Employee
NXP Employee

Hi Muthuraj

typical value is 30fps as shown on presentation p.21

A Deep Dive into Image Processing for i.MX 6 Series Applications Processors

p.118 shows 60fps use case.

Performance depends om use case, since some IPU submodules are limited to 1920x1080 @ 30 fps,

sect.38.1.2.1.5.3 Image Converter (IC) IMX6SDLRM

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
860 Views
zhengl
Contributor II

If the resolution about 640x480 60fps and data format is RGB888 from mipi-csi2, is it possible to preview in 60fps?

0 Kudos