i.MX6 dual lite EPDC dual scan

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX6 dual lite EPDC dual scan

Jump to solution
776 Views
hiroyukihara
Contributor III

Hello,

I'm thinking of trying to create a dual monitor of EPD in i.MX6 dual lite. (EPDx2)
Split display the "two-screen" that was created in the app.
I think that trying to achieve by using the dual scan of EPDC.
However, since in this case one screen divided into two parts,
The output from the EPDC in the two cables I think that trying to output to the EPD.

Whether this method is possible?

Labels (1)
0 Kudos
1 Solution
473 Views
igorpadykov
NXP Employee
NXP Employee

Hi hiroyuki

I believe you are right, this could be feasible.

Best regards
igor
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
474 Views
igorpadykov
NXP Employee
NXP Employee

Hi hiroyuki

I believe you are right, this could be feasible.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos