i.MX6 automotive security support

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX6 automotive security support

Jump to solution
1,000 Views
ko-hey
Senior Contributor II

Hi all

I have a question about i.MX6 security features.

My customer have considered a CPU that it supports EVITA-Full(High).

The EVITA-Full is automotive security specification and it need some security modules.

Evita Specification ( http://www.evita-project.org )

Can i.MX6's seciruty modelus satisfy the EVITA-Full specification ?

According to the following presentation material in P45, it seems i.MX6 doesn't support EVITA-Full.

But I can not have conclusive evidence.

So please let me know.

http://cache.freescale.com/files/FTF_2015/ftf-acc-f1265.pdf?fsrch=1&sr=1&pageNum=1

Ko-hey

Labels (1)
0 Kudos
1 Solution
758 Views
jamesbone
NXP TechSupport
NXP TechSupport

Hello Ko-Hey

Yes unfortunately the i.Mx6 does not support EVITA High  specification  the device only achieve the EVITA Medium. You can get more details in the following link:

http://www.freescale.com/files/training/doc/dwf/DWF13_AMF_AUT_T0112_Detroit.pdf


Have a great day,
Jaime

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
3 Replies
759 Views
jamesbone
NXP TechSupport
NXP TechSupport

Hello Ko-Hey

Yes unfortunately the i.Mx6 does not support EVITA High  specification  the device only achieve the EVITA Medium. You can get more details in the following link:

http://www.freescale.com/files/training/doc/dwf/DWF13_AMF_AUT_T0112_Detroit.pdf


Have a great day,
Jaime

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
758 Views
ko-hey
Senior Contributor II

Hi Jaime

Thank you for your support.

Ko-hey

0 Kudos
671 Views
ko-hey
Senior Contributor II

Hi @jamesbone ,

 

I would like to get the doc that you linked in this thread.

Could you share it again ?

 

Ko-hey

0 Kudos