i.MX6 and jitter for audio

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX6 and jitter for audio

999 Views
philippev
Contributor I

Hi all, we use i.MX6 for audio application. i.MX6 generate master clock for bit rate like 44.1 for audio cd quality.

We use PLL4 (also referred to as an Audio PLL) - This is a fractional multiplier PLL used

for generating a low jitter and high precision audio clock with standardized audio

frequencies. The PLLs oscillator frequency range is from 650MHz to 1300MHz, and

the frequency resolution is better than 1Hz. This clock is mainly used as a clock for

serial audio interfaces and as a reference clock for external audio codecs. It is

equipped with a divider on its output and can generate divided by 1, 2 or 4 from the

PLL VCO frequency.

Question we have a low jitter, but we want to quantify this value (nano sec , pico sec) ?

Tks.


Labels (3)
0 Kudos
Reply
2 Replies

750 Views
sinanakman
Senior Contributor III

Hi Philippe, does this document help : cache.freescale.com/files/32bit/doc/app_note/AN4952.pdf 

Regards

Sinan Akman

0 Kudos
Reply

750 Views
philippev
Contributor I

tanks

0 Kudos
Reply