i.MX6 and i.MX8M WideVine drm support

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX6 and i.MX8M WideVine drm support

1,707 Views
qwang
Contributor I

Hi,

Can you please confirm if these two chipsets support WideVine drm? And which level of WideVine drm are they support, lvl 1 or lvl 3?

i.MX6:

NXP MCIMX6Q6AVT10AC (32-bit MPU, Quad ARM Cortex-A9 core, 1GHz processor)

i.MX8M:

NXP MIMX8MQ6CVAHZAB (64-bit MPU, Quad ARM Cortex-A53 core, 1.3GHz processor, HDR10)

Thanks.

Tags (2)
0 Kudos
1 Reply

1,480 Views
gusarambula
NXP TechSupport
NXP TechSupport

Hello Qingkui Wang,


The i.MX8M can support Widevine Level 1 in Android. There has been some work being done on this regard, although it’s handled through NXP Professional Services, so we do not have any public information on pricing we can share. (The i.MX8M should also be able to support it on Linux, although as far as I know there is less work involved in it as of today).
There is also some work on Widevine for the i.MX6.


I would need to ask you to please contact NXP Professional Services for more details.
https://www.nxp.com/support/support/nxp-professional-services:PROFESSIONAL-SERVICE


I hope this helps!
Regards,

0 Kudos