i.MX6 and SyncE

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX6 and SyncE

Jump to solution
2,428 Views
xav
Contributor II

Hi,

does i.MX6 SoloX allow to use SyncE ethernet ?

If not, does another i.MX chip allow it ? Or even the soon-to-be i.MX7 ?

Thanks,

        Xav

Tags (1)
0 Kudos
Reply
1 Solution
2,317 Views
igorpadykov
NXP Employee
NXP Employee

Hi Xavier

unfortunately i.MX6SX, iMX7 do not support in

hardware SyncE. I am not aware of future chips

where it will be supported.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
5 Replies
2,318 Views
igorpadykov
NXP Employee
NXP Employee

Hi Xavier

unfortunately i.MX6SX, iMX7 do not support in

hardware SyncE. I am not aware of future chips

where it will be supported.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply
2,317 Views
xav
Contributor II

Hi Igor,

OK, I understand. Is it possible to still have SyncE by adding a different PHY, which will replace the built-in one ?

0 Kudos
Reply
2,317 Views
igorpadykov
NXP Employee
NXP Employee

Hi Xavier

I am afraid not, because except PHY, it should be also supported by i.MX MAC.

~igor

0 Kudos
Reply
2,317 Views
xav
Contributor II

I'm not so sure, this PHY DP83640 | PHY | Ethernet | Description & parametrics  has been used on a Sitara AM335x and make it support SyncE, which I don't think it does natively.

Would it be usable on an i.MX ?

0 Kudos
Reply
2,317 Views
xav
Contributor II

Would adding a dedicated PCIe ethernet chip work ?

0 Kudos
Reply