i.MX6 VoiP

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX6 VoiP

1,997 Views
Deejay
Contributor III

Hi,

Does Freescale have any white paper, application notes, reference designs on VoiP based on i.MX6?

Can they provide Linux source code for VoiP for the i.MX6 ?

Planning on using Yocto BSP.

http://www.iwavesystems.com/v2ip-on-iwaves-imx6-pico-itx-board

Thanks.

Devan

Labels (1)
0 Kudos
3 Replies

815 Views
igorpadykov
NXP Employee
NXP Employee

Hi Devian

sorry Linux source code for VoiP is not available, but it can be obtained

from third parties

iWave has provided V2IP on iWave’s Pico ITX i.MX6 | iWave Systems's Blog

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos

815 Views
Deejay
Contributor III

Hi Igor,

Thanks for your response...appreciate it very much.

How about app notes or ref design materials? are there any? Thanks again.

Rgds,

Devan

0 Kudos

815 Views
igorpadykov
NXP Employee
NXP Employee

Hi Devian

one can look at reference designs below

SABRE|Automotive-Infotainment|i.MX6|Freescale

SABRE for Smart Devices Reference Design|Freescale

Best regards

igor

0 Kudos