i.MX6 VPU encoder feature

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX6 VPU encoder feature

Jump to solution
2,352 Views
torus1000
Contributor V

Hi Chip Experts,

I think typical surveillance IP camera today supports 1080p30+D1 of h264@BP encoding.
So I want to confirm i.MX6S VPU H264 encoder features.
Compared to the i.MX6SDL RM Rev1 and Rev2, VPU feature updated as following.

Rev1: It can also perform H.264 BP/CBP, ... encoding up to @30fps.
          VPU can support encode or decode multiple video clips with multiple standards simultaneously.

Rev2: The supported resolution is up to ... full-HD 1920x1088@30fps for encoding ...
          VPU can support ...and also support multiple decoding and ...

(Q) Can i.MX6S VPU support multiple H264 encoding?
(Q) If yes, can i.MX6S VPU support 1920x1088@30fps plus D1@30fps H264 encoding?
(Q) Can i.MX6DLor6Q VPU support 1920x1088@30fps plus D1@30fps H264 encoding?

Thanks

Labels (2)
Tags (3)
0 Kudos
Reply
1 Solution
1,443 Views
Yuri
NXP Employee
NXP Employee

The VPU of the i.MX6 can decode two streams of 1080p@30 for MPEG4 / H.264.

  The VPU of the i.MX6 can encode single stream of 1080p@30 for MPEG4 / H.264.

 

  The VPU of the i.MX6 can decode four streams of 720p@30 for MPEG4 / H.264.

  The VPU of the i.MX6 can encode three streams of 720p@30 for MPEG4 / H.264.

We cannot guarantee 1920x1088@30fps plus D1@30fps H264 encoding.


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
1,444 Views
Yuri
NXP Employee
NXP Employee

The VPU of the i.MX6 can decode two streams of 1080p@30 for MPEG4 / H.264.

  The VPU of the i.MX6 can encode single stream of 1080p@30 for MPEG4 / H.264.

 

  The VPU of the i.MX6 can decode four streams of 720p@30 for MPEG4 / H.264.

  The VPU of the i.MX6 can encode three streams of 720p@30 for MPEG4 / H.264.

We cannot guarantee 1920x1088@30fps plus D1@30fps H264 encoding.


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply