i.MX6 VPU can encode/decode h.264 without software's help?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

i.MX6 VPU can encode/decode h.264 without software's help?

916 次查看
satoshishimoda
Senior Contributor I

Hi community,

I want to confirm the VPU behavior.
Which is correct?

1) VPU can do all h.264 encoding/decoding process by itself without software's help.
2) VPU is a general purpose processor likes DSP, so VPU runs only arithmetic processing and software is needed to handle H.264 format.

This information is needed to judge whehter h.264 license agreement is needed when use i.MX6 with VPU.


Best Regards,
Satoshi Shimoda

标签 (5)
标记 (1)
0 项奖励
回复
1 回复

672 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Satoshi

correct is 1), software just initializes VPU and provides

necessary parameters for its operation. More info can be found

on below presentation

Q&A: MX6 VPU H.264 Dual Stream Encode Limits

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复