i.MX6 VDD_SNVS_IN input voltage levels

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

i.MX6 VDD_SNVS_IN input voltage levels

跳至解决方案
3,011 次查看
martin-schad
Contributor I

Hello,

I have a theoretical question related to the VDD_SNVS_IN maximum input voltage level.

Wandboard and Sabre Lite designs connect VDD_HIGH_IN and VDD_SNVS_IN inputs together and supply

both from a regulator 3.3V (±2%) rail without problems. This is a straightforward solution if the coincell

features of the iMX6 (or the PCMIC MMPF0100) are not needed.

Standard 3.3V power supplies have an output tolerance of about ±2% (ATX specifies ±5% for the 3.3V rail).

Therefore the VDD_SNVS_IN pin may "see" up to 3.465V (for 5% tolerance) or 3.366V (for 2% tolerance)

under worst case conditions when connected to a "typical" 3.3V rail.

But the iMX6 Solo/Dual Lite Data sheet specifies the following absolute maximum ratings:

- VDD_HIGH_IN input voltage: 3.6V

- VDD_SNVS_IN input voltage: 3.3V

Because the Sabre Lite and Wandboard solutions are working, I have the following question:

Can VDD_SNVS_IN input withstand 3.465V (if and only if it is connected to the VDD_HIGH_IN pin)

or is it required to keep the 3.3V rail below 3.3V under all circumstances, which means that we in fact need

a 3.0V...3.2V power source to supply VDD_SNVS_IN and VDD_HIGH_IN input pair ?

I don't understand the reason why the VDD_SNVS_IN input can tolerate 3.3V only while the VDD_HIGH_IN

input can tolerate up to 3.6V. They are internally connected with a bypass. Has this something to do with

the coincell charger electronics inside the iMX6 ?

Regards,

Martin.

标签 (1)
0 项奖励
回复
1 解答
2,026 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Martin

yes VDD_SNVS_IN input can withstand 3.465V,

however reliability characteristics are guaranteed only under

datasheet conditions (up to 3.3V).

Seems one can add small schottky diode for lowering voltage.

Best regards

chip

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
1 回复
2,027 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Martin

yes VDD_SNVS_IN input can withstand 3.465V,

however reliability characteristics are guaranteed only under

datasheet conditions (up to 3.3V).

Seems one can add small schottky diode for lowering voltage.

Best regards

chip

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复