i.MX6 ULL based device sometimes can't open USB camera

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

i.MX6 ULL based device sometimes can't open USB camera

1,015 次查看
kevinw25
Contributor I

We are attempting to debug an issue that we are seeing with the 6/100 devices we are working with. The issue is that a UVC camera passed QA at the device manufacturer (took a photo), but now some of those devices constantly cannot open the UVC camera anymore.

With the devices that no longer take photos we get messages as shown below in the kernel log:

[ 20.153600] usb 1-1: new high-speed USB device number 2 using ci_hdrc
[ 20.398490] usb 1-1: unable to read config index 0 descriptor/all
[ 20.403538] usb 1-1: can't read configurations, error -32
[ 20.543572] usb 1-1: new high-speed USB device number 3 using ci_hdrc
[ 20.746370] usb 1-1: device descriptor read/all, error -71
[ 20.883987] usb 1-1: new high-speed USB device number 4 using ci_hdrc
[ 21.333593] usb 1-1: device not accepting address 4, error -71

 

some other devices will show


[ 20.243591] usb 1-1: new high-speed USB device number 2 using ci_hdrc
[ 20.448903] usb 1-1: unable to read config index 0 descriptor/start: -32
[ 20.454553] usb 1-1: chopping to 0 config(s)
[ 20.478077] usb 1-1: no configuration chosen from 0 choices

On  the 94 functioning devices we see this instead

[ 19.933590] usb 1-1: new high-speed USB device number 2 using ci_hdrc
[ 20.294390] uvcvideo: Found UVC 1.00 device MikrOkularFullHD (053a:9230)
[ 20.308968] input: MikrOkularFullHD as /devices/soc0/soc/2100000.aips-bus/2184200.usb/ci_hdrc.1/usb1/1-1/1-1:1.0/input/input1
[ 20.320578] evbug: Connected device: input1 (MikrOkularFullHD at usb-ci_hdrc.1-1/button)
[ 20.327982] usbcore: registered new interface driver uvcvideo
[ 20.332528] USB Video Class driver (1.1.1)


We've tried rebooting the device, leaving it off for a few minutes then turning it back on (in case overcurrent was the issue) - but none of that has worked so far.

We are running Linux version 4.9.11-1.0.0+gc27010d

Any ideas on why this would be happening to a small portion of the devices we received ? And why it would have worked once and then stopped ?

标签 (2)
标记 (3)
0 项奖励
回复
1 回复

904 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Kevin

one can try usb certification tests on bad devices

I.MX6 series USB Certification Guides 

Tweak usb signals using sect.4.3.3.1 General controls—USBPHY_CTRL register AN4589

https://www.nxp.com/docs/en/application-note/AN4589.pdf 

as signal may be weak due to board noise (or noisy environment, long cables) or power supplies ripples.

Also it may be ESD damaged, one can try to replace processors.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复