i.MX6 UL: loading image on OCRAM using Mfg tool

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX6 UL: loading image on OCRAM using Mfg tool

1,844件の閲覧回数
prabhatkumar
Contributor II

Hi,

I am using i.MX6 UL EVK dev kit. I was wondering, how to load u-boot image on OCRAM using Mfg tool. I can't find any document related to this.  I would like to test this on the dev kit.

ラベル(3)
タグ(3)
0 件の賞賛
返信
3 返答(返信)

1,382件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello

   We do not have OCRAM image of U_boot, at least because

of size : U-boot takes about 400 KB, OCRAM size is 128 KB.

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

1,382件の閲覧回数
prabhatkumar
Contributor II

Thanks for the quick reply.  Is it possible to load a piece of code on OCRAM using manufacturing tool to get the board from brick to configured state? Then I can use the configure state to load image on External RAM or other boot devices.

0 件の賞賛
返信

1,382件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

    Yes, basically it is possible to load a piece of code on OCRAM using manufacturing
tool. At least two points should be taken here for careful considerations :
1) loaded image should contain the IVT ;
2) OCRAM in itself used by boot ROM during load, therefore
   only area, mentioned as "OCRAM Free Area" in i.MX6 RM, section
   8.4.1 (Internal ROM /RAM memory map) is available for application.

u-boot.bin and u-boot.imx 

Also, please look at "Manufacturing Tool V2 UCL User Guide.docx" in MFG documentation.

Regards,

Yuri.

0 件の賞賛
返信