i.MX6 UL - Using the plugin can you write to the GPIO registers

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX6 UL - Using the plugin can you write to the GPIO registers

Jump to solution
1,495 Views
martintownsend
Contributor I

Hi,

We would like to assert a GPIO within 300ms of boot but we found that the time it takes to load U-Boot into memory takes longer than this.  The i.MX6 UltraLite Reference Manual states that the DCD can't address the GPIO registers so we can't use this method but there is no mention of allowed address ranges when using the Plugin.  I took a look at the existing plugins in the U-Boot source code and they all write to register address ranges that are only allowed for the DCD.  Does anyone know if any address range restrictions apply to plugins?

Many Thanks,

Martin.

Labels (2)
0 Kudos
Reply
1 Solution
1,383 Views
igorpadykov
NXP Employee
NXP Employee

Hi Martin

such restrictions do not apply to plugins, one can write to gpio registers.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
2 Replies
1,383 Views
martintownsend
Contributor I

Hi Igor,

I've just tried and can confirm that you can write to the GPIO registers.

Many Thanks,

Martin.

0 Kudos
Reply
1,384 Views
igorpadykov
NXP Employee
NXP Employee

Hi Martin

such restrictions do not apply to plugins, one can write to gpio registers.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply