i.MX6-UL/PF300x Orcad/Altium Symbol

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX6-UL/PF300x Orcad/Altium Symbol

1,633 Views
ulrichschmidt
Contributor I

Dear Freescale Support Community,

to start with a i.MX6-UL design, can you provide me with the symbol data to edit the schematics for the

- i.MX6-UL (14x14) and

- PF300x

Design tool is Altium, so if you can export from Orcad 16.2 is highly appreciated.

Best regards,

Uli

Labels (1)
0 Kudos
Reply
2 Replies

943 Views
art
NXP Employee
NXP Employee

Please find attached the schematic of the iMX6UL EVK CPU module in OrCAD 16.2 format where the symbol can be extracted from. Unfortunately, no OrCAD schematic of the PF3000 EVM board is available in public access.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

943 Views
marco_cassol
NXP Employee
NXP Employee

Hi Uli,

Create a Service Request under Sales and Support|Freescale  to request the information you need.

Please copy me as CC to it.

Regards,

Marco

0 Kudos
Reply