i.MX6 Thermal ?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX6 Thermal ?

1,200件の閲覧回数
Chicago1984
Contributor II

Looking at a thermal table on the imx6, there are junction to case and junction to package top resistances.  Is the package top some internal, inaccessible feature and in a normal situation I need to use junction-case?  What is the point of putting junction to package top?

ラベル(1)
0 件の賞賛
1 返信

540件の閲覧回数
Yuri
NXP Employee
NXP Employee

  Please look at section 3 [Psi-jt (Ψjt) Junction-to-Top of Package] of the next app note
for some details about Junction-to-Top of Package parameters.

http://www.ti.com/lit/an/spra953b/spra953b.pdf

The app note AN4579 provides useful thermal considerations.

AN4579 (i.MX 6 Series Thermal Management Guidelines)

http://cache.freescale.com/files/32bit/doc/app_note/AN4579.pdf


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛