i.MX6 Thermal fuse data Dispersion

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX6 Thermal fuse data Dispersion

Jump to solution
1,459 Views
mamorukanou
Contributor IV

Hi,  Support Teams

We check the i.MX6 thermal temp. calibration fuse data.

[sample 1]

CPU: Freescale i.MX6 family TO1.1 at 792 MHz

Thermal sensor with ratio = 172

Temperature:   34 C, calibration data 0x5424aa7d

[sample2]

CPU: Freescale i.MX6 family TO1.1 at 792 MHz

Thermal sensor with ratio = 172

Temperature:   32 C, calibration data 0x5444af7d

[Sample3]

CPU: Freescale i.MX6 family TO1.3 at 792 MHz

Thermal sensor with ratio = 179

Temperature:   33 C, calibration data 0x5704bf7d

Has calibration data been measured and written individually (one bye one), not for each lot ?

Best Regards,

kanou

Labels (1)
0 Kudos
Reply
1 Solution
1,305 Views
gusarambula
NXP TechSupport
NXP TechSupport

Hello Kanou,

I confirmed that the calibration points are measured during the manufacturing testing and are programmed in the fuse registers for each device, so each device will have its specific calibration value programmed based on the temperature. This is fused into the device as shown on the Table 1 of the AN5215.

I hope this information helps!

Regards,

View solution in original post

2 Replies
1,306 Views
gusarambula
NXP TechSupport
NXP TechSupport

Hello Kanou,

I confirmed that the calibration points are measured during the manufacturing testing and are programmed in the fuse registers for each device, so each device will have its specific calibration value programmed based on the temperature. This is fused into the device as shown on the Table 1 of the AN5215.

I hope this information helps!

Regards,

1,305 Views
gusarambula
NXP TechSupport
NXP TechSupport

Hello Kanou,

Application note 5215 covers the thermal management in detail.

https://www.nxp.com/docs/en/application-note/AN5215.pdf

I’m double checking whether this calibration is made by batch, wafer or unit and I’ll let you know when I find more information.

Regards,

0 Kudos
Reply