i.MX6 SoloX: to what extend pin compatible with i.MX6 S/DL/Q?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX6 SoloX: to what extend pin compatible with i.MX6 S/DL/Q?

554 Views
hroosen
Contributor I

Hi,

To what extend will the i.MX6 SoloX be pin compatible with i.MX6 Solo, DualLight or Quad?

The intention is to design a board which can be populated with i.MX6 SoloX and various other versions of i.MX6. I understand there will be differences with pins of some of the (additional) peripherals. But what about the rest (power, ddr-interface, ...) ?

Thanks,
Henri

Labels (1)
0 Kudos
1 Reply

361 Views
Yuri
NXP Employee
NXP Employee

Hello, Henri !

  The i.MX6 SoloX is NOT pin-to-pin compatible with i.MX6 Q/D/S/DL/SL.

Only software compatibility is provided.


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

Pin-to-pin

0 Kudos