i.MX6 SoloX RGMII signal timing original and internal delay

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX6 SoloX RGMII signal timing original and internal delay

Jump to solution
816 Views
m_c
Senior Contributor I

In page 94 i.MX6 SoloX data sheet <http://www.freescale.com/files/32bit/doc/data_sheet/IMX6SXAEC.pdf>, there are figure 55 & 56 shows timing original and internal delay. May we know how to change this timing mode?

Labels (1)
0 Kudos
1 Solution
612 Views
igorpadykov
NXP Employee
NXP Employee

Hi mc

note, figure 55 & 56 are the same as 54,55 IMX6DQCEC (rev.4,7/2015).pdf.

The i.MX6 Datasheet(s) do not provide the setup and hold timings, assuming using

the delay parameters. RGMII specs allow implementation of a delay on TXC or RXC

inside a transmitter.

To operate correctly :

TskewT max of MAC should be less than TskewR min of PHY.

TskewT max of PHY should be less than TskewR min of MAC.

Next, according to the i.MX6 Datasheet :

PC board design will require clocks to be routed such that an additional trace

delay of greater than 1.2 ns and less than 1.7 ns will be added to the

associated clock signal.

Best regards

igor
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
613 Views
igorpadykov
NXP Employee
NXP Employee

Hi mc

note, figure 55 & 56 are the same as 54,55 IMX6DQCEC (rev.4,7/2015).pdf.

The i.MX6 Datasheet(s) do not provide the setup and hold timings, assuming using

the delay parameters. RGMII specs allow implementation of a delay on TXC or RXC

inside a transmitter.

To operate correctly :

TskewT max of MAC should be less than TskewR min of PHY.

TskewT max of PHY should be less than TskewR min of MAC.

Next, according to the i.MX6 Datasheet :

PC board design will require clocks to be routed such that an additional trace

delay of greater than 1.2 ns and less than 1.7 ns will be added to the

associated clock signal.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos