i.MX6 Solo/DL XTALO pin capacitance

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX6 Solo/DL XTALO pin capacitance

1,343 Views
nexy_sm
Contributor II

Hi all,

I am not able to find input capacitance for XTALO pin. For XTALI there is a simulated value of 5pF but for XTAL) the same information is missing. Are they identical?

Labels (2)
0 Kudos
Reply
7 Replies

1,223 Views
igorpadykov
NXP Employee
NXP Employee

Hi Nemanja

these parameters can be found in ibis model i.MX 6DualLIte and i.MX 6Solo IBIS Model File(REV 1.4.)

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

1,223 Views
nexy_sm
Contributor II

Hi Igor,

I looked the IBIS model, but my knowledge in this area was literally zero until few hours ago. Still I do not see how to extract the capacitance value. The model gives Cpin for every pin but also package capacitance, and as far as I understood the answer lies in combining the two. Do you maybe have some hints?

Added later: The model for XTALI, XTALO and few other pins is NC, which somehow implies to not connected although I might be wrong. The truth is that for NC model there is no data given within the IBIS model.

Thank you,

Nemanja

0 Kudos
Reply

1,223 Views
igorpadykov
NXP Employee
NXP Employee

Hi Nemanja

you are right, ibis file gives capacitance for every pin and C_pkg, summer of two

is overall capacitance.

Best regards
igor

0 Kudos
Reply

1,223 Views
nexy_sm
Contributor II

Hi Igor,

this is rather way to wide range of values. For example:

[Package]
| variable      typ                 min                 max                 
R_pkg           0.2530623           0.0058833           0.551064            
L_pkg           3.74331nH           0.16939nH           6.95671nH           
C_pkg           7.39741pF           0.46418pF           134.527pF           
|
[Pin] signal_name        model_name      R_pin     L_pin     C_pin    
A2    PCIE_REXT                NC      0.448162  5.85114nH 1.30819pF
A3    PCIE_TXM                 NC      0.429313  5.53139nH 1.3572pF
A4    GND                      GND        NA        NA        NA       
A5    FA_ANA                   NC      0.403754  5.32197nH 1.15199pF
A6    USB_OTG_DP            usbdpdm    0.423339  5.05699nH 1.36064pF
A7    XTALI                    NC      0.351992  4.21633nH 1.18245pF

Cpkg goes as high as 134pF.

For other models (or for models because NC is maybe not a model) they provide Ccomp which is as I understood the capacitance seen from die to the pad.

So is there any more precise information about XTALI and XTALO capacitances?

0 Kudos
Reply

1,223 Views
igorpadykov
NXP Employee
NXP Employee

Hi Nemanja

recommended to use typical value.

>So is there any more precise information about XTALI and XTALO capacitances?

not, sorry.

Best regards
igor

0 Kudos
Reply

1,223 Views
nexy_sm
Contributor II

Hi Igor,

the problem is the datasheet gives typ. value for XTALI of about 5pF. Information for XTALO is rather missing. So IBIS model is of no big help here.

I wonder how other people chose load capacitors for their crystals.

0 Kudos
Reply

1,223 Views
igorpadykov
NXP Employee
NXP Employee

Hi Nemanja

if you are speaking about Table 22. XTALI and RTC_XTALI DC Parameters

i.MX 6Solo/6DualLite Applications Processors for Consumer Products (

it shows "Simulated data". While ibis model provides data obtained from factory tests.

One can follow Table 2-7. Oscillator and clock recommendations i.MX6 System Development User’s Guide

https://www.nxp.com/docs/en/user-guide/IMX6DQ6SDLHDG.pdf

Best regards
igor

0 Kudos
Reply