i.MX6 Sabre Board for small devices - CAN Bus (FlexCAN) available ?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

i.MX6 Sabre Board for small devices - CAN Bus (FlexCAN) available ?

1,195 次查看
torstenkoch
Contributor I

Hello !

We bought the Sabre Board for small devices with the QuadCore i.MX6. Now we want to use the CAN Bus. On the PCB, it is marked but no connector is assembled.

Is it possible to mount a 9-pole connector to the board and use the CAN ?  Or is CAN not available on this board ?

Thanks !

Torsten

标签 (5)
标记 (4)
0 项奖励
回复
1 回复

594 次查看
david_babin
NXP Employee
NXP Employee

Hi,

Yes, CAN is available on this board. The CAN chip is already installed. However, the DB-9 connector was intentionally not installed to reduce the cost of the kit. You may install a DB-9 connector and use CAN. Note that depending on your application, you may need to install the bias resistor and/or capacitor on the CAN_SPLT net.