i.MX6 Sabre Board for small devices - CAN Bus (FlexCAN) available ?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX6 Sabre Board for small devices - CAN Bus (FlexCAN) available ?

1,062 Views
torstenkoch
Contributor I

Hello !

We bought the Sabre Board for small devices with the QuadCore i.MX6. Now we want to use the CAN Bus. On the PCB, it is marked but no connector is assembled.

Is it possible to mount a 9-pole connector to the board and use the CAN ?  Or is CAN not available on this board ?

Thanks !

Torsten

Labels (5)
Tags (4)
0 Kudos
1 Reply

461 Views
david_babin
NXP Employee
NXP Employee

Hi,

Yes, CAN is available on this board. The CAN chip is already installed. However, the DB-9 connector was intentionally not installed to reduce the cost of the kit. You may install a DB-9 connector and use CAN. Note that depending on your application, you may need to install the bias resistor and/or capacitor on the CAN_SPLT net.