i.MX6 SPI maximum frequency in bi-directionnal com.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX6 SPI maximum frequency in bi-directionnal com.

ソリューションへジャンプ
1,900件の閲覧回数
nvassal
Contributor I

Hello iMx experts,

in IMX6SDLIEC document I've found that the SPI is limited to ~23MHz when reading, acting wether slave or device.

Even if the write operation can reach +60MHz ... does it means that, when operating in bi-direction, the whole SPI communication is limited to this low 23MHz?

 

Thanks for your help,

Kind regards,

Nicolas

0 件の賞賛
返信
1 解決策
1,892件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi nvasal

 

>when operating in bi-direction, the whole SPI communication is limited to this low 23MHz?

 

yes this is correct.

 

Best regards
igor

元の投稿で解決策を見る

2 返答(返信)
1,888件の閲覧回数
terry_lv
NXP Employee
NXP Employee

Hi,

  What do you mean by bi-direction? SPI can work in full duplex mode, that is, send and receive data at the same time.

  In my experience, when working in slave mode, ecspi in i.MX6 is using PIO mode. So it might not be able to support high SCK.

  The master mode should support 23MHz SCK.

  Thanks!

Regards

Terry

1,893件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi nvasal

 

>when operating in bi-direction, the whole SPI communication is limited to this low 23MHz?

 

yes this is correct.

 

Best regards
igor