i.MX6 Quad 4G RAM porting issue

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

i.MX6 Quad 4G RAM porting issue

2,282 次查看
wangvictor
Contributor III

Hi All,

I'm trying to porting 4G RAM on my board.

Now I have finished the stress test and put the value to the path of "u-boot-imx/2015.04-r0/git/board/freescale/mx6sabresd/mx6q_4x_mt41j128.cfg".

Below is the content of mx6q_4x_mt41j128.cfg.

/*
* Copyright (C) 2011-2014 Freescale Semiconductor, Inc.
* Jason Liu <[email protected]>
*
* SPDX-License-Identifier: GPL-2.0+
*
* Refer doc/README.imximage for more details about how-to configure
* and create imximage boot image
*
* The syntax is taken as close as possible with the kwbimage
*/

#define __ASSEMBLY__
#include <config.h>
/* image version */
IMAGE_VERSION 2

/*
* Boot Device : one of spi, sd, sata
* the board has no nand and eimnor
* spinor: flash_offset: 0x0400
* sata: flash_offset: 0x0400
* sd/mmc: flash_offset: 0x0400
*/

/* the same flash_offset as sd */
BOOT_FROM sd

#ifdef CONFIG_USE_PLUGIN
/*PLUGIN plugin-binary-file IRAM_FREE_START_ADDR*/
PLUGIN board/freescale/mx6sabresd/plugin.bin 0x00907000
#else

#ifdef CONFIG_SECURE_BOOT
CSF CONFIG_CSF_SIZE
#endif

/*
* Device Configuration Data (DCD)
*
* Each entry must have the format:
* Addr-type Address Value
*
* where:
* Addr-type register length (1,2 or 4 bytes)
* Address absolute address of the register
* value value to be stored in the register
*/
DATA 4, 0x020e0798, 0x000C0000
DATA 4, 0x020e0758, 0x00000000
DATA 4, 0x020e0588, 0x00000028
DATA 4, 0x020e0594, 0x00000028
DATA 4, 0x020e056c, 0x00000028
DATA 4, 0x020e0578, 0x00000028
DATA 4, 0x020e074c, 0x00000028
DATA 4, 0x020e057c, 0x00000028
DATA 4, 0x020e058c, 0x00000000
DATA 4, 0x020e059c, 0x00000028
DATA 4, 0x020e05a0, 0x00000028
DATA 4, 0x020e078c, 0x00000028
DATA 4, 0x020e0750, 0x00020000
DATA 4, 0x020e05a8, 0x00000028
DATA 4, 0x020e05b0, 0x00000028
DATA 4, 0x020e0524, 0x00000028
DATA 4, 0x020e051c, 0x00000028
DATA 4, 0x020e0518, 0x00000028
DATA 4, 0x020e050c, 0x00000028
DATA 4, 0x020e05b8, 0x00000028
DATA 4, 0x020e05c0, 0x00000028
DATA 4, 0x020e0774, 0x00020000
DATA 4, 0x020e0784, 0x00000028
DATA 4, 0x020e0788, 0x00000028
DATA 4, 0x020e0794, 0x00000028
DATA 4, 0x020e079c, 0x00000028
DATA 4, 0x020e07a0, 0x00000028
DATA 4, 0x020e07a4, 0x00000028
DATA 4, 0x020e07a8, 0x00000028
DATA 4, 0x020e0748, 0x00000028
DATA 4, 0x020e05ac, 0x00000028
DATA 4, 0x020e05b4, 0x00000028
DATA 4, 0x020e0528, 0x00000028
DATA 4, 0x020e0520, 0x00000028
DATA 4, 0x020e0514, 0x00000028
DATA 4, 0x020e0510, 0x00000028
DATA 4, 0x020e05bc, 0x00000028
DATA 4, 0x020e05c4, 0x00000028
DATA 4, 0x021b0800, 0xA1390003
DATA 4, 0x021b080c, 0x002C0030
DATA 4, 0x021b0810, 0x003B0037
DATA 4, 0x021b480c, 0x002C003C
DATA 4, 0x021b4810, 0x001A003A
DATA 4, 0x021b083c, 0x03300340
DATA 4, 0x021b0840, 0x032C0328
DATA 4, 0x021b483c, 0x033C034C
DATA 4, 0x021b4840, 0x0330027C
DATA 4, 0x021b0848, 0x3E34323A
DATA 4, 0x021b4848, 0x38343242
DATA 4, 0x021b0850, 0x34363E3A
DATA 4, 0x021b4850, 0x4232443E
DATA 4, 0x021b081c, 0x33333333
DATA 4, 0x021b0820, 0x33333333
DATA 4, 0x021b0824, 0x33333333
DATA 4, 0x021b0828, 0x33333333
DATA 4, 0x021b481c, 0x33333333
DATA 4, 0x021b4820, 0x33333333
DATA 4, 0x021b4824, 0x33333333
DATA 4, 0x021b4828, 0x33333333
DATA 4, 0x021b08b8, 0x00000800
DATA 4, 0x021b48b8, 0x00000800
DATA 4, 0x021b0004, 0x00020036
DATA 4, 0x021b0008, 0x09444040
DATA 4, 0x021b000c, 0xB8BE7955
DATA 4, 0x021b0010, 0xFF328F64
DATA 4, 0x021b0014, 0x01FF00DB
DATA 4, 0x021b0018, 0x00011740
DATA 4, 0x021b001c, 0x00008000
DATA 4, 0x021b002c, 0x000026D2
DATA 4, 0x021b0030, 0x008E1023
DATA 4, 0x021b0040, 0x0000007F
DATA 4, 0x021b0000, 0x853A0000
DATA 4, 0x021b001c, 0x02088032
DATA 4, 0x021b001c, 0x00008033
DATA 4, 0x021b001c, 0x00048031
DATA 4, 0x021b001c, 0x19408030
DATA 4, 0x021b001c, 0x04008040
DATA 4, 0x021b0020, 0x00007800
DATA 4, 0x021b0818, 0x00022227
DATA 4, 0x021b4818, 0x00022227
DATA 4, 0x021b0004, 0x00025576
DATA 4, 0x021b0404, 0x00011006
DATA 4, 0x021b001c, 0x00000000

/* set the default clock gate to save power */
DATA 4, 0x020c4068, 0x00C03F3F
DATA 4, 0x020c406c, 0x0030FC03
DATA 4, 0x020c4070, 0x0FFFC000
DATA 4, 0x020c4074, 0x3FF00000
DATA 4, 0x020c4078, 0x00FFF300
DATA 4, 0x020c407c, 0x0F0000F3
DATA 4, 0x020c4080, 0x000003FF

/* enable AXI cache for VDOA/VPU/IPU */
DATA 4, 0x020e0010, 0xF00000CF
/* set IPU AXI-id0 Qos=0xf(bypass) AXI-id1 Qos=0x7 */
DATA 4, 0x020e0018, 0x007F007F
DATA 4, 0x020e001c, 0x007F007F

/*
* Setup CCM_CCOSR register as follows:
*
* cko1_en = 1 --> CKO1 enabled
* cko1_div = 111 --> divide by 8
* cko1_sel = 1011 --> ahb_clk_root
*
* This sets CKO1 at ahb_clk_root/8 = 132/8 = 16.5 MHz
*/
DATA 4, 0x020c4060, 0x000000fb
#endif

And I modify this file too."u-boot-imx/2015.04-r0/git/arch/arm/include/asm/arch-mx6/imx-regs.h"

/*
* Copyright (C) 2011-2015 Freescale Semiconductor, Inc. All Rights Reserved.
*
* SPDX-License-Identifier: GPL-2.0+
*/

#ifndef __ASM_ARCH_MX6_IMX_REGS_H__
#define __ASM_ARCH_MX6_IMX_REGS_H__

#define ARCH_MXC

#ifdef CONFIG_MX6UL
#define CONFIG_SYS_CACHELINE_SIZE 64
#else
#define CONFIG_SYS_CACHELINE_SIZE 32
#endif

#define ROMCP_ARB_BASE_ADDR 0x00000000
#define ROMCP_ARB_END_ADDR 0x000FFFFF

#ifdef CONFIG_MX6SL
#define GPU_2D_ARB_BASE_ADDR 0x02200000
#define GPU_2D_ARB_END_ADDR 0x02203FFF
#define OPENVG_ARB_BASE_ADDR 0x02204000
#define OPENVG_ARB_END_ADDR 0x02207FFF

#elif (defined(CONFIG_MX6SX) || defined(CONFIG_MX6UL))
#define CAAM_ARB_BASE_ADDR 0x00100000
#define CAAM_ARB_END_ADDR 0x00107FFF
#define GPU_ARB_BASE_ADDR 0x01800000
#define GPU_ARB_END_ADDR 0x01803FFF
#define APBH_DMA_ARB_BASE_ADDR 0x01804000
#define APBH_DMA_ARB_END_ADDR 0x0180BFFF
#define M4_BOOTROM_BASE_ADDR 0x007F8000

#define MXS_APBH_BASE APBH_DMA_ARB_BASE_ADDR
#define MXS_GPMI_BASE (APBH_DMA_ARB_BASE_ADDR + 0x02000)
#define MXS_BCH_BASE (APBH_DMA_ARB_BASE_ADDR + 0x04000)

#else
#define CAAM_ARB_BASE_ADDR 0x00100000
#define CAAM_ARB_END_ADDR 0x00103FFF
#define APBH_DMA_ARB_BASE_ADDR 0x00110000
#define APBH_DMA_ARB_END_ADDR 0x00117FFF
#define HDMI_ARB_BASE_ADDR 0x00120000
#define HDMI_ARB_END_ADDR 0x00128FFF
#define GPU_3D_ARB_BASE_ADDR 0x00130000
#define GPU_3D_ARB_END_ADDR 0x00133FFF
#define GPU_2D_ARB_BASE_ADDR 0x00134000
#define GPU_2D_ARB_END_ADDR 0x00137FFF
#define DTCP_ARB_BASE_ADDR 0x00138000
#define DTCP_ARB_END_ADDR 0x0013BFFF

#define MXS_APBH_BASE APBH_DMA_ARB_BASE_ADDR
#define MXS_GPMI_BASE (APBH_DMA_ARB_BASE_ADDR + 0x02000)
#define MXS_BCH_BASE (APBH_DMA_ARB_BASE_ADDR + 0x04000)

#endif /* CONFIG_MX6SL */

/* GPV - PL301 configuration ports */
#if (defined(CONFIG_MX6SL) || defined(CONFIG_MX6SX) || defined(CONFIG_MX6UL))
#define GPV2_BASE_ADDR 0x00D00000
#else
#define GPV2_BASE_ADDR 0x00200000
#endif

#if (defined(CONFIG_MX6SX) || defined(CONFIG_MX6UL))
#define GPV3_BASE_ADDR 0x00E00000
#define GPV4_BASE_ADDR 0x00F00000
#define GPV5_BASE_ADDR 0x01000000
#define GPV6_BASE_ADDR 0x01100000
#define PCIE_ARB_BASE_ADDR 0x08000000
#define PCIE_ARB_END_ADDR 0x08FFFFFF
#else
#define GPV3_BASE_ADDR 0x00300000
#define GPV4_BASE_ADDR 0x00800000
#define PCIE_ARB_BASE_ADDR 0x01000000
#define PCIE_ARB_END_ADDR 0x01FFFFFF
#endif

#define IRAM_BASE_ADDR 0x00900000
#define SCU_BASE_ADDR 0x00A00000
#define IC_INTERFACES_BASE_ADDR 0x00A00100
#define GLOBAL_TIMER_BASE_ADDR 0x00A00200
#define PRIVATE_TIMERS_WD_BASE_ADDR 0x00A00600
#define IC_DISTRIBUTOR_BASE_ADDR 0x00A01000
#define L2_PL310_BASE 0x00A02000
#define GPV0_BASE_ADDR 0x00B00000
#define GPV1_BASE_ADDR 0x00C00000

#define AIPS1_ARB_BASE_ADDR 0x02000000
#define AIPS1_ARB_END_ADDR 0x020FFFFF
#define AIPS2_ARB_BASE_ADDR 0x02100000
#define AIPS2_ARB_END_ADDR 0x021FFFFF
#if (defined(CONFIG_MX6SX) || defined(CONFIG_MX6UL))
#define AIPS3_ARB_BASE_ADDR 0x02200000
#define AIPS3_ARB_END_ADDR 0x022FFFFF
#define WEIM_ARB_BASE_ADDR 0x50000000
#define WEIM_ARB_END_ADDR 0x57FFFFFF
#define QSPI1_ARB_BASE_ADDR 0x60000000
#define QSPI1_ARB_END_ADDR 0x6FFFFFFF
#define QSPI2_ARB_BASE_ADDR 0x70000000
#define QSPI2_ARB_END_ADDR 0x7FFFFFFF
#else
#define SATA_ARB_BASE_ADDR 0x02200000
#define SATA_ARB_END_ADDR 0x02203FFF
#define OPENVG_ARB_BASE_ADDR 0x02204000
#define OPENVG_ARB_END_ADDR 0x02207FFF
#define HSI_ARB_BASE_ADDR 0x02208000
#define HSI_ARB_END_ADDR 0x0220BFFF
#define IPU1_ARB_BASE_ADDR 0x02400000
#define IPU1_ARB_END_ADDR 0x027FFFFF
#define IPU2_ARB_BASE_ADDR 0x02800000
#define IPU2_ARB_END_ADDR 0x02BFFFFF
#define WEIM_ARB_BASE_ADDR 0x08000000
#define WEIM_ARB_END_ADDR 0x0FFFFFFF
#endif

#if (defined(CONFIG_MX6SL) || defined(CONFIG_MX6SX) || defined(CONFIG_MX6UL))
#define MMDC0_ARB_BASE_ADDR 0x80000000
#define MMDC0_ARB_END_ADDR 0xFFFFFFFF
#define MMDC1_ARB_BASE_ADDR 0xC0000000
#define MMDC1_ARB_END_ADDR 0xFFFFFFFF
#else
#define MMDC0_ARB_BASE_ADDR 0x10000000
#define MMDC0_ARB_END_ADDR 0x7FFFFFFF
#define MMDC1_ARB_BASE_ADDR 0x80000000
#define MMDC1_ARB_END_ADDR 0xFFFFFFFF
#endif

#if (!(defined(CONFIG_MX6SX) || defined(CONFIG_MX6UL)))
#define IPU_SOC_BASE_ADDR IPU1_ARB_BASE_ADDR
#define IPU_SOC_OFFSET 0x00200000
#endif

/* Defines for Blocks connected via AIPS (SkyBlue) */
#define ATZ1_BASE_ADDR AIPS1_ARB_BASE_ADDR
#define ATZ2_BASE_ADDR AIPS2_ARB_BASE_ADDR
#define AIPS1_BASE_ADDR AIPS1_ON_BASE_ADDR
#define AIPS2_BASE_ADDR AIPS2_ON_BASE_ADDR

#define SPDIF_BASE_ADDR (ATZ1_BASE_ADDR + 0x04000)
#define ECSPI1_BASE_ADDR (ATZ1_BASE_ADDR + 0x08000)
#define ECSPI2_BASE_ADDR (ATZ1_BASE_ADDR + 0x0C000)
#define ECSPI3_BASE_ADDR (ATZ1_BASE_ADDR + 0x10000)
#define ECSPI4_BASE_ADDR (ATZ1_BASE_ADDR + 0x14000)
#ifdef CONFIG_MX6SL
#define UART5_IPS_BASE_ADDR (ATZ1_BASE_ADDR + 0x18000)
#define UART1_IPS_BASE_ADDR (ATZ1_BASE_ADDR + 0x20000)
#define UART2_IPS_BASE_ADDR (ATZ1_BASE_ADDR + 0x24000)
#define SSI1_IPS_BASE_ADDR (ATZ1_BASE_ADDR + 0x28000)
#define SSI2_IPS_BASE_ADDR (ATZ1_BASE_ADDR + 0x2C000)
#define SSI3_IPS_BASE_ADDR (ATZ1_BASE_ADDR + 0x30000)
#define UART3_IPS_BASE_ADDR (ATZ1_BASE_ADDR + 0x34000)
#define UART4_IPS_BASE_ADDR (ATZ1_BASE_ADDR + 0x38000)
#else

#if defined(CONFIG_MX6UL)
#define UART7_IPS_BASE_ADDR (ATZ1_BASE_ADDR + 0x18000)
#elif !defined(CONFIG_MX6SX)
#define ECSPI5_BASE_ADDR (ATZ1_BASE_ADDR + 0x18000)
#endif

#define UART1_BASE (ATZ1_BASE_ADDR + 0x20000)
#if defined(CONFIG_MX6UL)
#define UART8_IPS_BASE_ADDR (ATZ1_BASE_ADDR + 0x24000)
#define SAI1_BASE_ADDR (ATZ1_BASE_ADDR + 0x28000)
#define SAI2_BASE_ADDR (ATZ1_BASE_ADDR + 0x2C000)
#define SAI3_BASE_ADDR (ATZ1_BASE_ADDR + 0x30000)
#else
#define ESAI1_BASE_ADDR (ATZ1_BASE_ADDR + 0x24000)
#define SSI1_BASE_ADDR (ATZ1_BASE_ADDR + 0x28000)
#define SSI2_BASE_ADDR (ATZ1_BASE_ADDR + 0x2C000)
#define SSI3_BASE_ADDR (ATZ1_BASE_ADDR + 0x30000)
#endif
#define ASRC_BASE_ADDR (ATZ1_BASE_ADDR + 0x34000)
#endif

#if defined(CONFIG_MX6UL)
#define TOUCH_CTRL_BASE_ADDR (ATZ1_BASE_ADDR + 0x40000)
#define BEE_BASE_ADDR (ATZ1_BASE_ADDR + 0x44000)
#elif !defined(CONFIG_MX6SX)
#define SPBA_BASE_ADDR (ATZ1_BASE_ADDR + 0x3C000)
#define VPU_BASE_ADDR (ATZ1_BASE_ADDR + 0x40000)
#endif
#define AIPS1_ON_BASE_ADDR (ATZ1_BASE_ADDR + 0x7C000)

#define AIPS1_OFF_BASE_ADDR (ATZ1_BASE_ADDR + 0x80000)
#define PWM1_BASE_ADDR (AIPS1_OFF_BASE_ADDR + 0x0000)
#define PWM2_BASE_ADDR (AIPS1_OFF_BASE_ADDR + 0x4000)
#define PWM3_BASE_ADDR (AIPS1_OFF_BASE_ADDR + 0x8000)
#define PWM4_BASE_ADDR (AIPS1_OFF_BASE_ADDR + 0xC000)
#define CAN1_BASE_ADDR (AIPS1_OFF_BASE_ADDR + 0x10000)
#define CAN2_BASE_ADDR (AIPS1_OFF_BASE_ADDR + 0x14000)
#define GPT1_BASE_ADDR (AIPS1_OFF_BASE_ADDR + 0x18000)
#define GPIO1_BASE_ADDR (AIPS1_OFF_BASE_ADDR + 0x1C000)
#define GPIO2_BASE_ADDR (AIPS1_OFF_BASE_ADDR + 0x20000)
#define GPIO3_BASE_ADDR (AIPS1_OFF_BASE_ADDR + 0x24000)
#define GPIO4_BASE_ADDR (AIPS1_OFF_BASE_ADDR + 0x28000)
#define GPIO5_BASE_ADDR (AIPS1_OFF_BASE_ADDR + 0x2C000)
#if defined(CONFIG_MX6UL)
#define SNVS_LP_BASE_ADDR (AIPS1_OFF_BASE_ADDR + 0x30000)
#define ENET2_BASE_ADDR (AIPS1_OFF_BASE_ADDR + 0x34000)
#else
#define GPIO6_BASE_ADDR (AIPS1_OFF_BASE_ADDR + 0x30000)
#define GPIO7_BASE_ADDR (AIPS1_OFF_BASE_ADDR + 0x34000)
#endif
#define KPP_BASE_ADDR (AIPS1_OFF_BASE_ADDR + 0x38000)
#define WDOG1_BASE_ADDR (AIPS1_OFF_BASE_ADDR + 0x3C000)
#define WDOG2_BASE_ADDR (AIPS1_OFF_BASE_ADDR + 0x40000)
#define ANATOP_BASE_ADDR (AIPS1_OFF_BASE_ADDR + 0x48000)
#define USB_PHY0_BASE_ADDR (AIPS1_OFF_BASE_ADDR + 0x49000)
#define USB_PHY1_BASE_ADDR (AIPS1_OFF_BASE_ADDR + 0x4a000)
#define CCM_BASE_ADDR (AIPS1_OFF_BASE_ADDR + 0x44000)
#define SNVS_BASE_ADDR (AIPS1_OFF_BASE_ADDR + 0x4C000)
#define EPIT1_BASE_ADDR (AIPS1_OFF_BASE_ADDR + 0x50000)
#define EPIT2_BASE_ADDR (AIPS1_OFF_BASE_ADDR + 0x54000)
#define SRC_BASE_ADDR (AIPS1_OFF_BASE_ADDR + 0x58000)
#define GPC_BASE_ADDR (AIPS1_OFF_BASE_ADDR + 0x5C000)
#define IOMUXC_BASE_ADDR (AIPS1_OFF_BASE_ADDR + 0x60000)
#define IOMUXC_GPR_BASE_ADDR (AIPS1_OFF_BASE_ADDR + 0x64000)
#if defined(CONFIG_MX6SL)
#define CSI_BASE_ADDR (AIPS1_OFF_BASE_ADDR + 0x64000)
#define SIPIX_BASE_ADDR (AIPS1_OFF_BASE_ADDR + 0x68000)
#define SDMA_PORT_HOST_BASE_ADDR (AIPS1_OFF_BASE_ADDR + 0x6C000)

#elif defined(CONFIG_MX6SX)
#define CANFD1_BASE_ADDR (AIPS1_OFF_BASE_ADDR + 0x68000)
#define SDMA_BASE_ADDR (AIPS1_OFF_BASE_ADDR + 0x6C000)
#define CANFD2_BASE_ADDR (AIPS1_OFF_BASE_ADDR + 0x70000)
#define SEMAPHORE1_BASE_ADDR (AIPS1_OFF_BASE_ADDR + 0x74000)
#define SEMAPHORE2_BASE_ADDR (AIPS1_OFF_BASE_ADDR + 0x78000)
#define RDC_BASE_ADDR (AIPS1_OFF_BASE_ADDR + 0x7C000)

#elif defined(CONFIG_MX6UL)
#define GPT2_BASE_ADDR (AIPS1_OFF_BASE_ADDR + 0x68000)
#define SDMA_BASE_ADDR (AIPS1_OFF_BASE_ADDR + 0x6C000)
#define PWM5_BASE_ADDR (AIPS1_OFF_BASE_ADDR + 0x70000)
#define PWM6_BASE_ADDR (AIPS1_OFF_BASE_ADDR + 0x74000)
#define PWM7_BASE_ADDR (AIPS1_OFF_BASE_ADDR + 0x78000)
#define PWM8_BASE_ADDR (AIPS1_OFF_BASE_ADDR + 0x7C000)
#else
#define DCIC1_BASE_ADDR (AIPS1_OFF_BASE_ADDR + 0x64000)
#define DCIC2_BASE_ADDR (AIPS1_OFF_BASE_ADDR + 0x68000)
#define DMA_REQ_PORT_HOST_BASE_ADDR (AIPS1_OFF_BASE_ADDR + 0x6C000)
#endif
#define EPDC_BASE_ADDR (AIPS1_OFF_BASE_ADDR + 0x74000)

#define AIPS2_ON_BASE_ADDR (ATZ2_BASE_ADDR + 0x7C000)
#define AIPS2_OFF_BASE_ADDR (ATZ2_BASE_ADDR + 0x80000)
#if defined(CONFIG_MX6UL)
#define CAAM_BASE_ADDR (ATZ2_BASE_ADDR + 0x40000)
#define ARM_BASE_ADDR (ATZ2_BASE_ADDR)
#else
#define CAAM_BASE_ADDR (ATZ2_BASE_ADDR)
#define ARM_BASE_ADDR (ATZ2_BASE_ADDR + 0x40000)
#endif
#define CONFIG_SYS_FSL_SEC_ADDR CAAM_BASE_ADDR
#define CONFIG_SYS_FSL_JR0_ADDR (CAAM_BASE_ADDR + 0x1000)

#define USB_PL301_BASE_ADDR (AIPS2_OFF_BASE_ADDR + 0x0000)
#define USB_BASE_ADDR (AIPS2_OFF_BASE_ADDR + 0x4000)

#define ENET_BASE_ADDR (AIPS2_OFF_BASE_ADDR + 0x8000)
#if defined(CONFIG_MX6SL)
#define MSHC_IPS_BASE_ADDR (AIPS2_OFF_BASE_ADDR + 0xC000)
#elif defined(CONFIG_MX6UL)
#define SIM1_IPS_BASE_ADDR (AIPS2_OFF_BASE_ADDR + 0xC000)
#else
#define MLB_BASE_ADDR (AIPS2_OFF_BASE_ADDR + 0xC000)
#endif

#define USDHC1_BASE_ADDR (AIPS2_OFF_BASE_ADDR + 0x10000)
#define USDHC2_BASE_ADDR (AIPS2_OFF_BASE_ADDR + 0x14000)
#if !defined(CONFIG_MX6UL)
#define USDHC3_BASE_ADDR (AIPS2_OFF_BASE_ADDR + 0x18000)
#define USDHC4_BASE_ADDR (AIPS2_OFF_BASE_ADDR + 0x1C000)
#else
#define ADC1_BASE_ADDR (AIPS2_OFF_BASE_ADDR + 0x18000)
#define ADC2_BASE_ADDR (AIPS2_OFF_BASE_ADDR + 0x1C000)
#endif
#define I2C1_BASE_ADDR (AIPS2_OFF_BASE_ADDR + 0x20000)
#define I2C2_BASE_ADDR (AIPS2_OFF_BASE_ADDR + 0x24000)
#define I2C3_BASE_ADDR (AIPS2_OFF_BASE_ADDR + 0x28000)
#define ROMCP_BASE_ADDR (AIPS2_OFF_BASE_ADDR + 0x2C000)
#define MMDC_P0_BASE_ADDR (AIPS2_OFF_BASE_ADDR + 0x30000)
#if defined(CONFIG_MX6SL)
#define RNGB_IPS_BASE_ADDR (AIPS2_OFF_BASE_ADDR + 0x34000)
#elif defined(CONFIG_MX6SX)
#define ENET2_BASE_ADDR (AIPS2_OFF_BASE_ADDR + 0x34000)
#elif defined(CONFIG_MX6UL)
#define SIM2_BASE_ADDR (AIPS2_OFF_BASE_ADDR + 0x34000)
#else
#define MMDC_P1_BASE_ADDR (AIPS2_OFF_BASE_ADDR + 0x34000)
#endif

#define WEIM_BASE_ADDR (AIPS2_OFF_BASE_ADDR + 0x38000)
#define OCOTP_BASE_ADDR (AIPS2_OFF_BASE_ADDR + 0x3C000)
#define CSU_BASE_ADDR (AIPS2_OFF_BASE_ADDR + 0x40000)
#if defined(CONFIG_MX6UL)
#define CSI_BASE_ADDR (AIPS2_OFF_BASE_ADDR + 0x44000)
#define LCDIF1_BASE_ADDR (AIPS2_OFF_BASE_ADDR + 0x48000)
#define LCDIF2_BASE_ADDR LCDIF1_BASE_ADDR
#define PXP_BASE_ADDR (AIPS2_OFF_BASE_ADDR + 0x4C000)
#else
#define IP2APB_PERFMON1_BASE_ADDR (AIPS2_OFF_BASE_ADDR + 0x44000)
#define IP2APB_PERFMON2_BASE_ADDR (AIPS2_OFF_BASE_ADDR + 0x48000)
#ifdef CONFIG_MX6SX
#define DEBUG_MONITOR_BASE_ADDR (AIPS2_OFF_BASE_ADDR + 0x4C000)
#else
#define IP2APB_PERFMON3_BASE_ADDR (AIPS2_OFF_BASE_ADDR + 0x4C000)
#endif
#endif /* CONFIG_MX6UL */

#define IP2APB_TZASC1_BASE_ADDR (AIPS2_OFF_BASE_ADDR + 0x50000)
#if defined(CONFIG_MX6UL)
#define SYSCNT_RD_IPS_BASE_ADDR (AIPS2_OFF_BASE_ADDR + 0x54000)
#define SYSCNT_CMP_IPS_BASE_ADDR (AIPS2_OFF_BASE_ADDR + 0x58000)
#define SYSCNT_CTRL_IPS_BASE_ADDR (AIPS2_OFF_BASE_ADDR + 0x5C000)
#define QSPI1_BASE_ADDR (AIPS2_OFF_BASE_ADDR + 0x60000)
#define WDOG3_BASE_ADDR (AIPS2_OFF_BASE_ADDR + 0x64000)
#elif defined(CONFIG_MX6SX)
#define SAI1_BASE_ADDR (AIPS2_OFF_BASE_ADDR + 0x54000)
#define AUDMUX_BASE_ADDR (AIPS2_OFF_BASE_ADDR + 0x58000)
#define SAI2_BASE_ADDR (AIPS2_OFF_BASE_ADDR + 0x5C000)
#define QSPI1_BASE_ADDR (AIPS2_OFF_BASE_ADDR + 0x60000)
#define QSPI2_BASE_ADDR (AIPS2_OFF_BASE_ADDR + 0x64000)
#else
#define IP2APB_TZASC2_BASE_ADDR (AIPS2_OFF_BASE_ADDR + 0x54000)
#define MIPI_CSI2_BASE_ADDR (AIPS2_OFF_BASE_ADDR + 0x5C000)
#define MIPI_DSI_BASE_ADDR (AIPS2_OFF_BASE_ADDR + 0x60000)
#define VDOA_BASE_ADDR (AIPS2_OFF_BASE_ADDR + 0x64000)
#endif
#define UART2_BASE (AIPS2_OFF_BASE_ADDR + 0x68000)
#define UART3_BASE (AIPS2_OFF_BASE_ADDR + 0x6C000)
#define UART4_BASE (AIPS2_OFF_BASE_ADDR + 0x70000)
#define UART5_BASE (AIPS2_OFF_BASE_ADDR + 0x74000)
#if defined(CONFIG_MX6SX)
#define I2C4_BASE_ADDR (AIPS2_OFF_BASE_ADDR + 0x78000)
#define QOSC_BASE_ADDR (AIPS2_OFF_BASE_ADDR + 0x7C000)
#elif defined(CONFIG_MX6UL)
#define I2C4_BASE_ADDR (AIPS2_OFF_BASE_ADDR + 0x78000)
#define UART6_BASE_ADDR (AIPS2_OFF_BASE_ADDR + 0x7C000)
#else
#define IP2APB_USBPHY1_BASE_ADDR (AIPS2_OFF_BASE_ADDR + 0x78000)
#define IP2APB_USBPHY2_BASE_ADDR (AIPS2_OFF_BASE_ADDR + 0x7C000)
#endif

#define OTG_BASE_ADDR USB_BASE_ADDR

#if defined(CONFIG_MX6UL)
#define SCTR_BASE_ADDR SYSCNT_CTRL_IPS_BASE_ADDR
#endif

#ifdef CONFIG_MX6SX
#define GIS_BASE_ADDR (AIPS3_ARB_BASE_ADDR + 0x04000)
#define DCIC1_BASE_ADDR (AIPS3_ARB_BASE_ADDR + 0x0C000)
#define DCIC2_BASE_ADDR (AIPS3_ARB_BASE_ADDR + 0x10000)
#define CSI1_BASE_ADDR (AIPS3_ARB_BASE_ADDR + 0x14000)
#define PXP_BASE_ADDR (AIPS3_ARB_BASE_ADDR + 0x18000)
#define CSI2_BASE_ADDR (AIPS3_ARB_BASE_ADDR + 0x1C000)
#define LCDIF1_BASE_ADDR (AIPS3_ARB_BASE_ADDR + 0x20000)
#define LCDIF2_BASE_ADDR (AIPS3_ARB_BASE_ADDR + 0x24000)
#define VADC_BASE_ADDR (AIPS3_ARB_BASE_ADDR + 0x28000)
#define VDEC_BASE_ADDR (AIPS3_ARB_BASE_ADDR + 0x2C000)
#define SPBA_BASE_ADDR (AIPS3_ARB_BASE_ADDR + 0x3C000)
#define AIPS3_CONFIG_BASE_ADDR (AIPS3_ARB_BASE_ADDR + 0x7C000)
#define ADC1_BASE_ADDR (AIPS3_ARB_BASE_ADDR + 0x80000)
#define ADC2_BASE_ADDR (AIPS3_ARB_BASE_ADDR + 0x84000)
#define WDOG3_BASE_ADDR (AIPS3_ARB_BASE_ADDR + 0x88000)
#define ECSPI5_BASE_ADDR (AIPS3_ARB_BASE_ADDR + 0x8C000)
#define HS_BASE_ADDR (AIPS3_ARB_BASE_ADDR + 0x90000)
#define MU_MCU_BASE_ADDR (AIPS3_ARB_BASE_ADDR + 0x94000)
#define CANFD_BASE_ADDR (AIPS3_ARB_BASE_ADDR + 0x98000)
#define MU_DSP_BASE_ADDR (AIPS3_ARB_BASE_ADDR + 0x9C000)
#define UART6_BASE_ADDR (AIPS3_ARB_BASE_ADDR + 0xA0000)
#define PWM5_BASE_ADDR (AIPS3_ARB_BASE_ADDR + 0xA4000)
#define PWM6_BASE_ADDR (AIPS3_ARB_BASE_ADDR + 0xA8000)
#define PWM7_BASE_ADDR (AIPS3_ARB_BASE_ADDR + 0xAC000)
#define PWM8_BASE_ADDR (AIPS3_ARB_BASE_ADDR + 0xB0000)
#endif

#define CHIP_REV_1_0 0x10
#define CHIP_REV_1_1 0x11
#define CHIP_REV_1_2 0x12
#define CHIP_REV_1_3 0x13
#define CHIP_REV_1_4 0x14
#define CHIP_REV_1_5 0x15
#define CHIP_REV_2_0 0x20
#if (!(defined(CONFIG_MX6SX) || defined(CONFIG_MX6UL)))
#define IRAM_SIZE 0x00040000
#else
#define IRAM_SIZE 0x00040000 /* 0x00010000 for 1G; 0x00020000 for 2G 0x00040000 for 4G*/
#endif
#define FEC_QUIRK_ENET_MAC
#define SNVS_LPGPR 0x68

#if !(defined(__KERNEL_STRICT_NAMES) || defined(__ASSEMBLY__))
#include <asm/types.h>

extern void imx_get_mac_from_fuse(int dev_id, unsigned char *mac);

#define SRC_SCR_CORE_1_RESET_OFFSET 14
#define SRC_SCR_CORE_1_RESET_MASK (1<<SRC_SCR_CORE_1_RESET_OFFSET)
#define SRC_SCR_CORE_2_RESET_OFFSET 15
#define SRC_SCR_CORE_2_RESET_MASK (1<<SRC_SCR_CORE_2_RESET_OFFSET)
#define SRC_SCR_CORE_3_RESET_OFFSET 16
#define SRC_SCR_CORE_3_RESET_MASK (1<<SRC_SCR_CORE_3_RESET_OFFSET)
#define SRC_SCR_CORE_1_ENABLE_OFFSET 22
#define SRC_SCR_CORE_1_ENABLE_MASK (1<<SRC_SCR_CORE_1_ENABLE_OFFSET)
#define SRC_SCR_CORE_2_ENABLE_OFFSET 23
#define SRC_SCR_CORE_2_ENABLE_MASK (1<<SRC_SCR_CORE_2_ENABLE_OFFSET)
#define SRC_SCR_CORE_3_ENABLE_OFFSET 24
#define SRC_SCR_CORE_3_ENABLE_MASK (1<<SRC_SCR_CORE_3_ENABLE_OFFSET)

/* WEIM registers */
struct weim {
u32 cs0gcr1;
u32 cs0gcr2;
u32 cs0rcr1;
u32 cs0rcr2;
u32 cs0wcr1;
u32 cs0wcr2;

u32 cs1gcr1;
u32 cs1gcr2;
u32 cs1rcr1;
u32 cs1rcr2;
u32 cs1wcr1;
u32 cs1wcr2;

u32 cs2gcr1;
u32 cs2gcr2;
u32 cs2rcr1;
u32 cs2rcr2;
u32 cs2wcr1;
u32 cs2wcr2;

u32 cs3gcr1;
u32 cs3gcr2;
u32 cs3rcr1;
u32 cs3rcr2;
u32 cs3wcr1;
u32 cs3wcr2;

u32 unused[12];

u32 wcr;
u32 wiar;
u32 ear;
};

/* System Reset Controller (SRC) */
struct src {
u32 scr;
u32 sbmr1;
u32 srsr;
u32 reserved1[2];
u32 sisr;
u32 simr;
u32 sbmr2;
u32 gpr1;
u32 gpr2;
u32 gpr3;
u32 gpr4;
u32 gpr5;
u32 gpr6;
u32 gpr7;
u32 gpr8;
u32 gpr9;
u32 gpr10;
};

/* GPR1 bitfields */
#define IOMUXC_GPR1_ENET_CLK_SEL_OFFSET 21
#define IOMUXC_GPR1_ENET_CLK_SEL_MASK (1 << IOMUXC_GPR1_ENET_CLK_SEL_OFFSET)
#define IOMUXC_GPR1_USB_OTG_ID_OFFSET 13
#define IOMUXC_GPR1_USB_OTG_ID_SEL_MASK (1 << IOMUXC_GPR1_USB_OTG_ID_OFFSET)

/* GPR3 bitfields */
#define IOMUXC_GPR3_GPU_DBG_OFFSET 29
#define IOMUXC_GPR3_GPU_DBG_MASK (3<<IOMUXC_GPR3_GPU_DBG_OFFSET)
#define IOMUXC_GPR3_BCH_WR_CACHE_CTL_OFFSET 28
#define IOMUXC_GPR3_BCH_WR_CACHE_CTL_MASK (1<<IOMUXC_GPR3_BCH_WR_CACHE_CTL_OFFSET)
#define IOMUXC_GPR3_BCH_RD_CACHE_CTL_OFFSET 27
#define IOMUXC_GPR3_BCH_RD_CACHE_CTL_MASK (1<<IOMUXC_GPR3_BCH_RD_CACHE_CTL_OFFSET)
#define IOMUXC_GPR3_uSDHCx_WR_CACHE_CTL_OFFSET 26
#define IOMUXC_GPR3_uSDHCx_WR_CACHE_CTL_MASK (1<<IOMUXC_GPR3_uSDHCx_WR_CACHE_CTL_OFFSET)
#define IOMUXC_GPR3_uSDHCx_RD_CACHE_CTL_OFFSET 25
#define IOMUXC_GPR3_uSDHCx_RD_CACHE_CTL_MASK (1<<IOMUXC_GPR3_uSDHCx_RD_CACHE_CTL_OFFSET)
#define IOMUXC_GPR3_OCRAM_CTL_OFFSET 21
#define IOMUXC_GPR3_OCRAM_CTL_MASK (0xf<<IOMUXC_GPR3_OCRAM_CTL_OFFSET)
#define IOMUXC_GPR3_OCRAM_STATUS_OFFSET 17
#define IOMUXC_GPR3_OCRAM_STATUS_MASK (0xf<<IOMUXC_GPR3_OCRAM_STATUS_OFFSET)
#define IOMUXC_GPR3_CORE3_DBG_ACK_EN_OFFSET 16
#define IOMUXC_GPR3_CORE3_DBG_ACK_EN_MASK (1<<IOMUXC_GPR3_CORE3_DBG_ACK_EN_OFFSET)
#define IOMUXC_GPR3_CORE2_DBG_ACK_EN_OFFSET 15
#define IOMUXC_GPR3_CORE2_DBG_ACK_EN_MASK (1<<IOMUXC_GPR3_CORE2_DBG_ACK_EN_OFFSET)
#define IOMUXC_GPR3_CORE1_DBG_ACK_EN_OFFSET 14
#define IOMUXC_GPR3_CORE1_DBG_ACK_EN_MASK (1<<IOMUXC_GPR3_CORE1_DBG_ACK_EN_OFFSET)
#define IOMUXC_GPR3_CORE0_DBG_ACK_EN_OFFSET 13
#define IOMUXC_GPR3_CORE0_DBG_ACK_EN_MASK (1<<IOMUXC_GPR3_CORE0_DBG_ACK_EN_OFFSET)
#define IOMUXC_GPR3_TZASC2_BOOT_LOCK_OFFSET 12
#define IOMUXC_GPR3_TZASC2_BOOT_LOCK_MASK (1<<IOMUXC_GPR3_TZASC2_BOOT_LOCK_OFFSET)
#define IOMUXC_GPR3_TZASC1_BOOT_LOCK_OFFSET 11
#define IOMUXC_GPR3_TZASC1_BOOT_LOCK_MASK (1<<IOMUXC_GPR3_TZASC1_BOOT_LOCK_OFFSET)
#define IOMUXC_GPR3_IPU_DIAG_OFFSET 10
#define IOMUXC_GPR3_IPU_DIAG_MASK (1<<IOMUXC_GPR3_IPU_DIAG_OFFSET)

#define IOMUXC_GPR3_MUX_SRC_IPU1_DI0 0
#define IOMUXC_GPR3_MUX_SRC_IPU1_DI1 1
#define IOMUXC_GPR3_MUX_SRC_IPU2_DI0 2
#define IOMUXC_GPR3_MUX_SRC_IPU2_DI1 3

#define IOMUXC_GPR3_LVDS1_MUX_CTL_OFFSET 8
#define IOMUXC_GPR3_LVDS1_MUX_CTL_MASK (3<<IOMUXC_GPR3_LVDS1_MUX_CTL_OFFSET)

#define IOMUXC_GPR3_LVDS0_MUX_CTL_OFFSET 6
#define IOMUXC_GPR3_LVDS0_MUX_CTL_MASK (3<<IOMUXC_GPR3_LVDS0_MUX_CTL_OFFSET)

#define IOMUXC_GPR3_MIPI_MUX_CTL_OFFSET 4
#define IOMUXC_GPR3_MIPI_MUX_CTL_MASK (3<<IOMUXC_GPR3_MIPI_MUX_CTL_OFFSET)

#define IOMUXC_GPR3_HDMI_MUX_CTL_OFFSET 2
#define IOMUXC_GPR3_HDMI_MUX_CTL_MASK (3<<IOMUXC_GPR3_HDMI_MUX_CTL_OFFSET)


struct iomuxc {
#if (defined(CONFIG_MX6SX) || defined(CONFIG_MX6UL))
u8 reserved[0x4000];
#endif

#ifdef CONFIG_MX6UL
u32 gpr[15];
#else
u32 gpr[14];
#endif
};

struct gpc {
u32 cntr;
u32 pgr;
u32 imr1;
u32 imr2;
u32 imr3;
u32 imr4;
u32 isr1;
u32 isr2;
u32 isr3;
u32 isr4;
};

#define IOMUXC_GPR2_COUNTER_RESET_VAL_OFFSET 20
#define IOMUXC_GPR2_COUNTER_RESET_VAL_MASK (3<<IOMUXC_GPR2_COUNTER_RESET_VAL_OFFSET)
#define IOMUXC_GPR2_LVDS_CLK_SHIFT_OFFSET 16
#define IOMUXC_GPR2_LVDS_CLK_SHIFT_MASK (7<<IOMUXC_GPR2_LVDS_CLK_SHIFT_OFFSET)

#define IOMUXC_GPR2_BGREF_RRMODE_OFFSET 15
#define IOMUXC_GPR2_BGREF_RRMODE_MASK (1<<IOMUXC_GPR2_BGREF_RRMODE_OFFSET)
#define IOMUXC_GPR2_BGREF_RRMODE_INTERNAL_RES (1<<IOMUXC_GPR2_BGREF_RRMODE_OFFSET)
#define IOMUXC_GPR2_BGREF_RRMODE_EXTERNAL_RES (0<<IOMUXC_GPR2_BGREF_RRMODE_OFFSET)
#define IOMUXC_GPR2_VSYNC_ACTIVE_HIGH 0
#define IOMUXC_GPR2_VSYNC_ACTIVE_LOW 1

#define IOMUXC_GPR2_DI1_VS_POLARITY_OFFSET 10
#define IOMUXC_GPR2_DI1_VS_POLARITY_MASK (1<<IOMUXC_GPR2_DI1_VS_POLARITY_OFFSET)
#define IOMUXC_GPR2_DI1_VS_POLARITY_ACTIVE_HIGH (IOMUXC_GPR2_VSYNC_ACTIVE_HIGH<<IOMUXC_GPR2_DI1_VS_POLARITY_OFFSET)
#define IOMUXC_GPR2_DI1_VS_POLARITY_ACTIVE_LOW (IOMUXC_GPR2_VSYNC_ACTIVE_LOW<<IOMUXC_GPR2_DI1_VS_POLARITY_OFFSET)

#define IOMUXC_GPR2_DI0_VS_POLARITY_OFFSET 9
#define IOMUXC_GPR2_DI0_VS_POLARITY_MASK (1<<IOMUXC_GPR2_DI0_VS_POLARITY_OFFSET)
#define IOMUXC_GPR2_DI0_VS_POLARITY_ACTIVE_HIGH (IOMUXC_GPR2_VSYNC_ACTIVE_HIGH<<IOMUXC_GPR2_DI0_VS_POLARITY_OFFSET)
#define IOMUXC_GPR2_DI0_VS_POLARITY_ACTIVE_LOW (IOMUXC_GPR2_VSYNC_ACTIVE_LOW<<IOMUXC_GPR2_DI0_VS_POLARITY_OFFSET)

#define IOMUXC_GPR2_BITMAP_SPWG 0
#define IOMUXC_GPR2_BITMAP_JEIDA 1

#define IOMUXC_GPR2_BIT_MAPPING_CH1_OFFSET 8
#define IOMUXC_GPR2_BIT_MAPPING_CH1_MASK (1<<IOMUXC_GPR2_BIT_MAPPING_CH1_OFFSET)
#define IOMUXC_GPR2_BIT_MAPPING_CH1_JEIDA (IOMUXC_GPR2_BITMAP_JEIDA<<IOMUXC_GPR2_BIT_MAPPING_CH1_OFFSET)
#define IOMUXC_GPR2_BIT_MAPPING_CH1_SPWG (IOMUXC_GPR2_BITMAP_SPWG<<IOMUXC_GPR2_BIT_MAPPING_CH1_OFFSET)

#define IOMUXC_GPR2_DATA_WIDTH_18 0
#define IOMUXC_GPR2_DATA_WIDTH_24 1

#define IOMUXC_GPR2_DATA_WIDTH_CH1_OFFSET 7
#define IOMUXC_GPR2_DATA_WIDTH_CH1_MASK (1<<IOMUXC_GPR2_DATA_WIDTH_CH1_OFFSET)
#define IOMUXC_GPR2_DATA_WIDTH_CH1_18BIT (IOMUXC_GPR2_DATA_WIDTH_18<<IOMUXC_GPR2_DATA_WIDTH_CH1_OFFSET)
#define IOMUXC_GPR2_DATA_WIDTH_CH1_24BIT (IOMUXC_GPR2_DATA_WIDTH_24<<IOMUXC_GPR2_DATA_WIDTH_CH1_OFFSET)

#define IOMUXC_GPR2_BIT_MAPPING_CH0_OFFSET 6
#define IOMUXC_GPR2_BIT_MAPPING_CH0_MASK (1<<IOMUXC_GPR2_BIT_MAPPING_CH0_OFFSET)
#define IOMUXC_GPR2_BIT_MAPPING_CH0_JEIDA (IOMUXC_GPR2_BITMAP_JEIDA<<IOMUXC_GPR2_BIT_MAPPING_CH0_OFFSET)
#define IOMUXC_GPR2_BIT_MAPPING_CH0_SPWG (IOMUXC_GPR2_BITMAP_SPWG<<IOMUXC_GPR2_BIT_MAPPING_CH0_OFFSET)

#define IOMUXC_GPR2_DATA_WIDTH_CH0_OFFSET 5
#define IOMUXC_GPR2_DATA_WIDTH_CH0_MASK (1<<IOMUXC_GPR2_DATA_WIDTH_CH0_OFFSET)
#define IOMUXC_GPR2_DATA_WIDTH_CH0_18BIT (IOMUXC_GPR2_DATA_WIDTH_18<<IOMUXC_GPR2_DATA_WIDTH_CH0_OFFSET)
#define IOMUXC_GPR2_DATA_WIDTH_CH0_24BIT (IOMUXC_GPR2_DATA_WIDTH_24<<IOMUXC_GPR2_DATA_WIDTH_CH0_OFFSET)

#define IOMUXC_GPR2_SPLIT_MODE_EN_OFFSET 4
#define IOMUXC_GPR2_SPLIT_MODE_EN_MASK (1<<IOMUXC_GPR2_SPLIT_MODE_EN_OFFSET)

#define IOMUXC_GPR2_MODE_DISABLED 0
#define IOMUXC_GPR2_MODE_ENABLED_DI0 1
#define IOMUXC_GPR2_MODE_ENABLED_DI1 3

#define IOMUXC_GPR2_LVDS_CH1_MODE_OFFSET 2
#define IOMUXC_GPR2_LVDS_CH1_MODE_MASK (3<<IOMUXC_GPR2_LVDS_CH1_MODE_OFFSET)
#define IOMUXC_GPR2_LVDS_CH1_MODE_DISABLED (IOMUXC_GPR2_MODE_DISABLED<<IOMUXC_GPR2_LVDS_CH1_MODE_OFFSET)
#define IOMUXC_GPR2_LVDS_CH1_MODE_ENABLED_DI0 (IOMUXC_GPR2_MODE_ENABLED_DI0<<IOMUXC_GPR2_LVDS_CH1_MODE_OFFSET)
#define IOMUXC_GPR2_LVDS_CH1_MODE_ENABLED_DI1 (IOMUXC_GPR2_MODE_ENABLED_DI1<<IOMUXC_GPR2_LVDS_CH1_MODE_OFFSET)

#define IOMUXC_GPR2_LVDS_CH0_MODE_OFFSET 0
#define IOMUXC_GPR2_LVDS_CH0_MODE_MASK (3<<IOMUXC_GPR2_LVDS_CH0_MODE_OFFSET)
#define IOMUXC_GPR2_LVDS_CH0_MODE_DISABLED (IOMUXC_GPR2_MODE_DISABLED<<IOMUXC_GPR2_LVDS_CH0_MODE_OFFSET)
#define IOMUXC_GPR2_LVDS_CH0_MODE_ENABLED_DI0 (IOMUXC_GPR2_MODE_ENABLED_DI0<<IOMUXC_GPR2_LVDS_CH0_MODE_OFFSET)
#define IOMUXC_GPR2_LVDS_CH0_MODE_ENABLED_DI1 (IOMUXC_GPR2_MODE_ENABLED_DI1<<IOMUXC_GPR2_LVDS_CH0_MODE_OFFSET)

#ifdef CONFIG_MX6SX
#define IMX6SX_GPR5_CSI1_MUX_CTRL_MASK (0x3 << 4)
#define IMX6SX_GPR5_CSI1_MUX_CTRL_EXT_PIN (0x0 << 4)
#define IMX6SX_GPR5_CSI1_MUX_CTRL_CVD (0x1 << 4)
#define IMX6SX_GPR5_CSI1_MUX_CTRL_VDAC_TO_CSI (0x2 << 4)
#define IMX6SX_GPR5_CSI1_MUX_CTRL_GND (0x3 << 4)
#endif

/* ECSPI registers */
struct cspi_regs {
u32 rxdata;
u32 txdata;
u32 ctrl;
u32 cfg;
u32 intr;
u32 dma;
u32 stat;
u32 period;
};

/*
* CSPI register definitions
*/
#define MXC_ECSPI
#define MXC_CSPICTRL_EN (1 << 0)
#define MXC_CSPICTRL_MODE (1 << 1)
#define MXC_CSPICTRL_XCH (1 << 2)
#define MXC_CSPICTRL_MODE_MASK (0xf << 4)
#define MXC_CSPICTRL_CHIPSELECT(x) (((x) & 0x3) << 12)
#define MXC_CSPICTRL_BITCOUNT(x) (((x) & 0xfff) << 20)
#define MXC_CSPICTRL_PREDIV(x) (((x) & 0xF) << 12)
#define MXC_CSPICTRL_POSTDIV(x) (((x) & 0xF) << 8)
#define MXC_CSPICTRL_SELCHAN(x) (((x) & 0x3) << 18)
#define MXC_CSPICTRL_MAXBITS 0xfff
#define MXC_CSPICTRL_TC (1 << 7)
#define MXC_CSPICTRL_RXOVF (1 << 6)
#define MXC_CSPIPERIOD_32KHZ (1 << 15)
#define MAX_SPI_BYTES 32
#if defined(CONFIG_MX6SL) || defined(CONFIG_MX6DL) || defined(CONFIG_MX6UL)
#define SPI_MAX_NUM 3
#else
#define SPI_MAX_NUM 4
#endif

/* Bit position inside CTRL register to be associated with SS */
#define MXC_CSPICTRL_CHAN 18

/* Bit position inside CON register to be associated with SS */
#define MXC_CSPICON_PHA 0 /* SCLK phase control */
#define MXC_CSPICON_POL 4 /* SCLK polarity */
#define MXC_CSPICON_SSPOL 12 /* SS polarity */
#define MXC_CSPICON_CTL 20 /* inactive state of SCLK */
#if defined(CONFIG_MX6SL) || defined(CONFIG_MX6DL) || defined(CONFIG_MX6UL)
#define MXC_SPI_BASE_ADDRESSES \
ECSPI1_BASE_ADDR, \
ECSPI2_BASE_ADDR, \
ECSPI3_BASE_ADDR, \
ECSPI4_BASE_ADDR
#else
#define MXC_SPI_BASE_ADDRESSES \
ECSPI1_BASE_ADDR, \
ECSPI2_BASE_ADDR, \
ECSPI3_BASE_ADDR, \
ECSPI4_BASE_ADDR, \
ECSPI5_BASE_ADDR
#endif

#define ANATOP_PLL_VIDEO 0xA0

struct ocotp_regs {
u32 ctrl;
u32 ctrl_set;
u32 ctrl_clr;
u32 ctrl_tog;
u32 timing;
u32 rsvd0[3];
u32 data;
u32 rsvd1[3];
u32 read_ctrl;
u32 rsvd2[3];
u32 read_fuse_data;
u32 rsvd3[3];
u32 sw_sticky;
u32 rsvd4[3];
u32 scs;
u32 scs_set;
u32 scs_clr;
u32 scs_tog;
u32 crc_addr;
u32 rsvd5[3];
u32 crc_value;
u32 rsvd6[3];
u32 version;
u32 rsvd7[0xdb];

/* fuse banks */
struct fuse_bank {
u32 fuse_regs[0x20];
} bank[0];
};

struct fuse_bank0_regs {
u32 lock;
u32 rsvd0[3];
u32 uid_low;
u32 rsvd1[3];
u32 uid_high;
u32 rsvd2[3];
u32 cfg2;
u32 rsvd3[3];
u32 cfg3;
u32 rsvd4[3];
u32 cfg4;
u32 rsvd5[3];
u32 cfg5;
u32 rsvd6[3];
u32 cfg6;
u32 rsvd7[3];
};

struct fuse_bank1_regs {
u32 mem[0x18];
u32 ana1;
u32 rsvd1[3];
u32 ana2;
u32 rsvd2[3];
};

#if (defined(CONFIG_MX6SX) || defined(CONFIG_MX6UL))
struct fuse_bank4_regs {
u32 sjc_resp_low;
u32 rsvd0[3];
u32 sjc_resp_high;
u32 rsvd1[3];
u32 mac_addr0;
u32 rsvd2[3];
u32 mac_addr1;
u32 rsvd3[3];
u32 mac_addr2;
u32 rsvd4[7];
u32 gp1;
u32 rsvd5[3];
u32 gp2;
u32 rsvd6[3];
};
#else
struct fuse_bank4_regs {
u32 sjc_resp_low;
u32 rsvd0[3];
u32 sjc_resp_high;
u32 rsvd1[3];
u32 mac_addr_low;
u32 rsvd2[3];
u32 mac_addr_high;
u32 rsvd3[0xb];
u32 gp1;
u32 rsvd4[3];
u32 gp2;
u32 rsvd5[3];
};
#endif

struct aipstz_regs {
u32 mprot0;
u32 mprot1;
u32 rsvd[0xe];
u32 opacr0;
u32 opacr1;
u32 opacr2;
u32 opacr3;
u32 opacr4;
};

struct anatop_regs {
u32 pll_sys; /* 0x000 */
u32 pll_sys_set; /* 0x004 */
u32 pll_sys_clr; /* 0x008 */
u32 pll_sys_tog; /* 0x00c */
u32 usb1_pll_480_ctrl; /* 0x010 */
u32 usb1_pll_480_ctrl_set; /* 0x014 */
u32 usb1_pll_480_ctrl_clr; /* 0x018 */
u32 usb1_pll_480_ctrl_tog; /* 0x01c */
u32 usb2_pll_480_ctrl; /* 0x020 */
u32 usb2_pll_480_ctrl_set; /* 0x024 */
u32 usb2_pll_480_ctrl_clr; /* 0x028 */
u32 usb2_pll_480_ctrl_tog; /* 0x02c */
u32 pll_528; /* 0x030 */
u32 pll_528_set; /* 0x034 */
u32 pll_528_clr; /* 0x038 */
u32 pll_528_tog; /* 0x03c */
u32 pll_528_ss; /* 0x040 */
u32 rsvd0[3];
u32 pll_528_num; /* 0x050 */
u32 rsvd1[3];
u32 pll_528_denom; /* 0x060 */
u32 rsvd2[3];
u32 pll_audio; /* 0x070 */
u32 pll_audio_set; /* 0x074 */
u32 pll_audio_clr; /* 0x078 */
u32 pll_audio_tog; /* 0x07c */
u32 pll_audio_num; /* 0x080 */
u32 rsvd3[3];
u32 pll_audio_denom; /* 0x090 */
u32 rsvd4[3];
u32 pll_video; /* 0x0a0 */
u32 pll_video_set; /* 0x0a4 */
u32 pll_video_clr; /* 0x0a8 */
u32 pll_video_tog; /* 0x0ac */
u32 pll_video_num; /* 0x0b0 */
u32 rsvd5[3];
u32 pll_video_denom; /* 0x0c0 */
u32 rsvd6[3];
u32 pll_mlb; /* 0x0d0 */
u32 pll_mlb_set; /* 0x0d4 */
u32 pll_mlb_clr; /* 0x0d8 */
u32 pll_mlb_tog; /* 0x0dc */
u32 pll_enet; /* 0x0e0 */
u32 pll_enet_set; /* 0x0e4 */
u32 pll_enet_clr; /* 0x0e8 */
u32 pll_enet_tog; /* 0x0ec */
u32 pfd_480; /* 0x0f0 */
u32 pfd_480_set; /* 0x0f4 */
u32 pfd_480_clr; /* 0x0f8 */
u32 pfd_480_tog; /* 0x0fc */
u32 pfd_528; /* 0x100 */
u32 pfd_528_set; /* 0x104 */
u32 pfd_528_clr; /* 0x108 */
u32 pfd_528_tog; /* 0x10c */
u32 reg_1p1; /* 0x110 */
u32 reg_1p1_set; /* 0x114 */
u32 reg_1p1_clr; /* 0x118 */
u32 reg_1p1_tog; /* 0x11c */
u32 reg_3p0; /* 0x120 */
u32 reg_3p0_set; /* 0x124 */
u32 reg_3p0_clr; /* 0x128 */
u32 reg_3p0_tog; /* 0x12c */
u32 reg_2p5; /* 0x130 */
u32 reg_2p5_set; /* 0x134 */
u32 reg_2p5_clr; /* 0x138 */
u32 reg_2p5_tog; /* 0x13c */
u32 reg_core; /* 0x140 */
u32 reg_core_set; /* 0x144 */
u32 reg_core_clr; /* 0x148 */
u32 reg_core_tog; /* 0x14c */
u32 ana_misc0; /* 0x150 */
u32 ana_misc0_set; /* 0x154 */
u32 ana_misc0_clr; /* 0x158 */
u32 ana_misc0_tog; /* 0x15c */
u32 ana_misc1; /* 0x160 */
u32 ana_misc1_set; /* 0x164 */
u32 ana_misc1_clr; /* 0x168 */
u32 ana_misc1_tog; /* 0x16c */
u32 ana_misc2; /* 0x170 */
u32 ana_misc2_set; /* 0x174 */
u32 ana_misc2_clr; /* 0x178 */
u32 ana_misc2_tog; /* 0x17c */
u32 tempsense0; /* 0x180 */
u32 tempsense0_set; /* 0x184 */
u32 tempsense0_clr; /* 0x188 */
u32 tempsense0_tog; /* 0x18c */
u32 tempsense1; /* 0x190 */
u32 tempsense1_set; /* 0x194 */
u32 tempsense1_clr; /* 0x198 */
u32 tempsense1_tog; /* 0x19c */
u32 usb1_vbus_detect; /* 0x1a0 */
u32 usb1_vbus_detect_set; /* 0x1a4 */
u32 usb1_vbus_detect_clr; /* 0x1a8 */
u32 usb1_vbus_detect_tog; /* 0x1ac */
u32 usb1_chrg_detect; /* 0x1b0 */
u32 usb1_chrg_detect_set; /* 0x1b4 */
u32 usb1_chrg_detect_clr; /* 0x1b8 */
u32 usb1_chrg_detect_tog; /* 0x1bc */
u32 usb1_vbus_det_stat; /* 0x1c0 */
u32 usb1_vbus_det_stat_set; /* 0x1c4 */
u32 usb1_vbus_det_stat_clr; /* 0x1c8 */
u32 usb1_vbus_det_stat_tog; /* 0x1cc */
u32 usb1_chrg_det_stat; /* 0x1d0 */
u32 usb1_chrg_det_stat_set; /* 0x1d4 */
u32 usb1_chrg_det_stat_clr; /* 0x1d8 */
u32 usb1_chrg_det_stat_tog; /* 0x1dc */
u32 usb1_loopback; /* 0x1e0 */
u32 usb1_loopback_set; /* 0x1e4 */
u32 usb1_loopback_clr; /* 0x1e8 */
u32 usb1_loopback_tog; /* 0x1ec */
u32 usb1_misc; /* 0x1f0 */
u32 usb1_misc_set; /* 0x1f4 */
u32 usb1_misc_clr; /* 0x1f8 */
u32 usb1_misc_tog; /* 0x1fc */
u32 usb2_vbus_detect; /* 0x200 */
u32 usb2_vbus_detect_set; /* 0x204 */
u32 usb2_vbus_detect_clr; /* 0x208 */
u32 usb2_vbus_detect_tog; /* 0x20c */
u32 usb2_chrg_detect; /* 0x210 */
u32 usb2_chrg_detect_set; /* 0x214 */
u32 usb2_chrg_detect_clr; /* 0x218 */
u32 usb2_chrg_detect_tog; /* 0x21c */
u32 usb2_vbus_det_stat; /* 0x220 */
u32 usb2_vbus_det_stat_set; /* 0x224 */
u32 usb2_vbus_det_stat_clr; /* 0x228 */
u32 usb2_vbus_det_stat_tog; /* 0x22c */
u32 usb2_chrg_det_stat; /* 0x230 */
u32 usb2_chrg_det_stat_set; /* 0x234 */
u32 usb2_chrg_det_stat_clr; /* 0x238 */
u32 usb2_chrg_det_stat_tog; /* 0x23c */
u32 usb2_loopback; /* 0x240 */
u32 usb2_loopback_set; /* 0x244 */
u32 usb2_loopback_clr; /* 0x248 */
u32 usb2_loopback_tog; /* 0x24c */
u32 usb2_misc; /* 0x250 */
u32 usb2_misc_set; /* 0x254 */
u32 usb2_misc_clr; /* 0x258 */
u32 usb2_misc_tog; /* 0x25c */
u32 digprog; /* 0x260 */
u32 reserved1[7];
u32 digprog_sololite; /* 0x280 */
};

#define ANATOP_PFD_FRAC_SHIFT(n) ((n)*8)
#define ANATOP_PFD_FRAC_MASK(n) (0x3f<<ANATOP_PFD_FRAC_SHIFT(n))
#define ANATOP_PFD_STABLE_SHIFT(n) (6+((n)*8))
#define ANATOP_PFD_STABLE_MASK(n) (1<<ANATOP_PFD_STABLE_SHIFT(n))
#define ANATOP_PFD_CLKGATE_SHIFT(n) (7+((n)*8))
#define ANATOP_PFD_CLKGATE_MASK(n) (1<<ANATOP_PFD_CLKGATE_SHIFT(n))

struct iomuxc_gpr_base_regs {
#if defined(CONFIG_MX6UL)
u32 gpr[15]; /* 0x000 */
#else
u32 gpr[14]; /* 0x000 */
#endif
};

struct iomuxc_base_regs {
#if !(defined(CONFIG_MX6SX) || defined(CONFIG_MX6UL))
u32 gpr[14]; /* 0x000 */
#endif
u32 obsrv[5]; /* 0x038 */
u32 swmux_ctl[197]; /* 0x04c */
u32 swpad_ctl[250]; /* 0x360 */
u32 swgrp[26]; /* 0x748 */
u32 daisy[104]; /* 0x7b0..94c */
};

struct wdog_regs {
u16 wcr; /* Control */
u16 wsr; /* Service */
u16 wrsr; /* Reset Status */
u16 wicr; /* Interrupt Control */
u16 wmcr; /* Miscellaneous Control */
};

#define PWMCR_PRESCALER(x) (((x - 1) & 0xFFF) << 4)
#define PWMCR_DOZEEN (1 << 24)
#define PWMCR_WAITEN (1 << 23)
#define PWMCR_DBGEN (1 << 22)
#define PWMCR_CLKSRC_IPG_HIGH (2 << 16)
#define PWMCR_CLKSRC_IPG (1 << 16)
#define PWMCR_EN (1 << 0)

struct pwm_regs {
u32 cr;
u32 sr;
u32 ir;
u32 sar;
u32 pr;
u32 cnr;
};

struct dbg_monitor_regs {
u32 ctrl[4]; /* Control */
u32 master_en[4]; /* Master enable */
u32 irq[4]; /* IRQ */
u32 trap_addr_low[4]; /* Trap address low */
u32 trap_addr_high[4]; /* Trap address high */
u32 trap_id[4]; /* Trap ID */
u32 snvs_addr[4]; /* SNVS address */
u32 snvs_data[4]; /* SNVS data */
u32 snvs_info[4]; /* SNVS info */
u32 version[4]; /* Version */
};

/* eLCDIF controller registers */
struct mxs_lcdif_regs {
u32 hw_lcdif_ctrl; /* 0x00 */
u32 hw_lcdif_ctrl_set;
u32 hw_lcdif_ctrl_clr;
u32 hw_lcdif_ctrl_tog;
u32 hw_lcdif_ctrl1; /* 0x10 */
u32 hw_lcdif_ctrl1_set;
u32 hw_lcdif_ctrl1_clr;
u32 hw_lcdif_ctrl1_tog;
u32 hw_lcdif_ctrl2; /* 0x20 */
u32 hw_lcdif_ctrl2_set;
u32 hw_lcdif_ctrl2_clr;
u32 hw_lcdif_ctrl2_tog;
u32 hw_lcdif_transfer_count; /* 0x30 */
u32 reserved1[3];
u32 hw_lcdif_cur_buf; /* 0x40 */
u32 reserved2[3];
u32 hw_lcdif_next_buf; /* 0x50 */
u32 reserved3[3];
u32 hw_lcdif_timing; /* 0x60 */
u32 reserved4[3];
u32 hw_lcdif_vdctrl0; /* 0x70 */
u32 hw_lcdif_vdctrl0_set;
u32 hw_lcdif_vdctrl0_clr;
u32 hw_lcdif_vdctrl0_tog;
u32 hw_lcdif_vdctrl1; /* 0x80 */
u32 reserved5[3];
u32 hw_lcdif_vdctrl2; /* 0x90 */
u32 reserved6[3];
u32 hw_lcdif_vdctrl3; /* 0xa0 */
u32 reserved7[3];
u32 hw_lcdif_vdctrl4; /* 0xb0 */
u32 reserved8[3];
u32 hw_lcdif_dvictrl0; /* 0xc0 */
u32 reserved9[3];
u32 hw_lcdif_dvictrl1; /* 0xd0 */
u32 reserved10[3];
u32 hw_lcdif_dvictrl2; /* 0xe0 */
u32 reserved11[3];
u32 hw_lcdif_dvictrl3; /* 0xf0 */
u32 reserved12[3];
u32 hw_lcdif_dvictrl4; /* 0x100 */
u32 reserved13[3];
u32 hw_lcdif_csc_coeffctrl0; /* 0x110 */
u32 reserved14[3];
u32 hw_lcdif_csc_coeffctrl1; /* 0x120 */
u32 reserved15[3];
u32 hw_lcdif_csc_coeffctrl2; /* 0x130 */
u32 reserved16[3];
u32 hw_lcdif_csc_coeffctrl3; /* 0x140 */
u32 reserved17[3];
u32 hw_lcdif_csc_coeffctrl4; /* 0x150 */
u32 reserved18[3];
u32 hw_lcdif_csc_offset; /* 0x160 */
u32 reserved19[3];
u32 hw_lcdif_csc_limit; /* 0x170 */
u32 reserved20[3];
u32 hw_lcdif_data; /* 0x180 */
u32 reserved21[3];
u32 hw_lcdif_bm_error_stat; /* 0x190 */
u32 reserved22[3];
u32 hw_lcdif_crc_stat; /* 0x1a0 */
u32 reserved23[3];
u32 hw_lcdif_lcdif_stat; /* 0x1b0 */
u32 reserved24[3];
u32 hw_lcdif_version; /* 0x1c0 */
u32 reserved25[3];
u32 hw_lcdif_debug0; /* 0x1d0 */
u32 reserved26[3];
u32 hw_lcdif_debug1; /* 0x1e0 */
u32 reserved27[3];
u32 hw_lcdif_debug2; /* 0x1f0 */
u32 reserved28[3];
u32 hw_lcdif_thres; /* 0x200 */
u32 reserved29[3];
u32 hw_lcdif_as_ctrl; /* 0x210 */
u32 reserved30[3];
u32 hw_lcdif_as_buf; /* 0x220 */
u32 reserved31[3];
u32 hw_lcdif_as_next_buf; /* 0x230 */
u32 reserved32[3];
u32 hw_lcdif_as_clrkeylow; /* 0x240 */
u32 reserved33[3];
u32 hw_lcdif_as_clrkeyhigh; /* 0x250 */
u32 reserved34[3];
u32 hw_lcdif_as_sync_delay; /* 0x260 */
u32 reserved35[3];
u32 hw_lcdif_as_debug3; /* 0x270 */
u32 reserved36[3];
u32 hw_lcdif_as_debug4; /* 0x280 */
u32 reserved37[3];
u32 hw_lcdif_as_debug5; /* 0x290 */
};

struct rdc_regs {
u32 vir; /* Version information */
u32 reserved1[8];
u32 stat; /* Status */
u32 intctrl; /* Interrupt and Control */
u32 intstat; /* Interrupt Status */
u32 reserved2[116];
u32 mda[32]; /* Master Domain Assignment */
u32 reserved3[96];
u32 pdap[104]; /* Peripheral Domain Access Permissions */
u32 reserved4[88];
struct {
u32 mrsa; /* Memory Region Start Address */
u32 mrea; /* Memory Region End Address */
u32 mrc; /* Memory Region Control */
u32 mrvs; /* Memory Region Violation Status */
} mem_region[55];
};

struct rdc_sema_regs {
u8 gate[64]; /* Gate */
u16 rstgt; /* Reset Gate */
};

#define MXS_LCDIF_BASE LCDIF2_BASE_ADDR

#define LCDIF_CTRL_SFTRST (1 << 31)
#define LCDIF_CTRL_CLKGATE (1 << 30)
#define LCDIF_CTRL_YCBCR422_INPUT (1 << 29)
#define LCDIF_CTRL_READ_WRITEB (1 << 28)
#define LCDIF_CTRL_WAIT_FOR_VSYNC_EDGE (1 << 27)
#define LCDIF_CTRL_DATA_SHIFT_DIR (1 << 26)
#define LCDIF_CTRL_SHIFT_NUM_BITS_MASK (0x1f << 21)
#define LCDIF_CTRL_SHIFT_NUM_BITS_OFFSET 21
#define LCDIF_CTRL_DVI_MODE (1 << 20)
#define LCDIF_CTRL_BYPASS_COUNT (1 << 19)
#define LCDIF_CTRL_VSYNC_MODE (1 << 18)
#define LCDIF_CTRL_DOTCLK_MODE (1 << 17)
#define LCDIF_CTRL_DATA_SELECT (1 << 16)
#define LCDIF_CTRL_INPUT_DATA_SWIZZLE_MASK (0x3 << 14)
#define LCDIF_CTRL_INPUT_DATA_SWIZZLE_OFFSET 14
#define LCDIF_CTRL_CSC_DATA_SWIZZLE_MASK (0x3 << 12)
#define LCDIF_CTRL_CSC_DATA_SWIZZLE_OFFSET 12
#define LCDIF_CTRL_LCD_DATABUS_WIDTH_MASK (0x3 << 10)
#define LCDIF_CTRL_LCD_DATABUS_WIDTH_OFFSET 10
#define LCDIF_CTRL_LCD_DATABUS_WIDTH_16BIT (0 << 10)
#define LCDIF_CTRL_LCD_DATABUS_WIDTH_8BIT (1 << 10)
#define LCDIF_CTRL_LCD_DATABUS_WIDTH_18BIT (2 << 10)
#define LCDIF_CTRL_LCD_DATABUS_WIDTH_24BIT (3 << 10)
#define LCDIF_CTRL_WORD_LENGTH_MASK (0x3 << 8)
#define LCDIF_CTRL_WORD_LENGTH_OFFSET 8
#define LCDIF_CTRL_WORD_LENGTH_16BIT (0 << 8)
#define LCDIF_CTRL_WORD_LENGTH_8BIT (1 << 8)
#define LCDIF_CTRL_WORD_LENGTH_18BIT (2 << 8)
#define LCDIF_CTRL_WORD_LENGTH_24BIT (3 << 8)
#define LCDIF_CTRL_RGB_TO_YCBCR422_CSC (1 << 7)
#define LCDIF_CTRL_LCDIF_MASTER (1 << 5)
#define LCDIF_CTRL_DATA_FORMAT_16_BIT (1 << 3)
#define LCDIF_CTRL_DATA_FORMAT_18_BIT (1 << 2)
#define LCDIF_CTRL_DATA_FORMAT_24_BIT (1 << 1)
#define LCDIF_CTRL_RUN (1 << 0)

#define LCDIF_CTRL1_COMBINE_MPU_WR_STRB (1 << 27)
#define LCDIF_CTRL1_BM_ERROR_IRQ_EN (1 << 26)
#define LCDIF_CTRL1_BM_ERROR_IRQ (1 << 25)
#define LCDIF_CTRL1_RECOVER_ON_UNDERFLOW (1 << 24)
#define LCDIF_CTRL1_INTERLACE_FIELDS (1 << 23)
#define LCDIF_CTRL1_START_INTERLACE_FROM_SECOND_FIELD (1 << 22)
#define LCDIF_CTRL1_FIFO_CLEAR (1 << 21)
#define LCDIF_CTRL1_IRQ_ON_ALTERNATE_FIELDS (1 << 20)
#define LCDIF_CTRL1_BYTE_PACKING_FORMAT_MASK (0xf << 16)
#define LCDIF_CTRL1_BYTE_PACKING_FORMAT_OFFSET 16
#define LCDIF_CTRL1_OVERFLOW_IRQ_EN (1 << 15)
#define LCDIF_CTRL1_UNDERFLOW_IRQ_EN (1 << 14)
#define LCDIF_CTRL1_CUR_FRAME_DONE_IRQ_EN (1 << 13)
#define LCDIF_CTRL1_VSYNC_EDGE_IRQ_EN (1 << 12)
#define LCDIF_CTRL1_OVERFLOW_IRQ (1 << 11)
#define LCDIF_CTRL1_UNDERFLOW_IRQ (1 << 10)
#define LCDIF_CTRL1_CUR_FRAME_DONE_IRQ (1 << 9)
#define LCDIF_CTRL1_VSYNC_EDGE_IRQ (1 << 8)
#define LCDIF_CTRL1_BUSY_ENABLE (1 << 2)
#define LCDIF_CTRL1_MODE86 (1 << 1)
#define LCDIF_CTRL1_RESET (1 << 0)

#define LCDIF_CTRL2_OUTSTANDING_REQS_MASK (0x7 << 21)
#define LCDIF_CTRL2_OUTSTANDING_REQS_OFFSET 21
#define LCDIF_CTRL2_OUTSTANDING_REQS_REQ_1 (0x0 << 21)
#define LCDIF_CTRL2_OUTSTANDING_REQS_REQ_2 (0x1 << 21)
#define LCDIF_CTRL2_OUTSTANDING_REQS_REQ_4 (0x2 << 21)
#define LCDIF_CTRL2_OUTSTANDING_REQS_REQ_8 (0x3 << 21)
#define LCDIF_CTRL2_OUTSTANDING_REQS_REQ_16 (0x4 << 21)
#define LCDIF_CTRL2_BURST_LEN_8 (1 << 20)
#define LCDIF_CTRL2_ODD_LINE_PATTERN_MASK (0x7 << 16)
#define LCDIF_CTRL2_ODD_LINE_PATTERN_OFFSET 16
#define LCDIF_CTRL2_ODD_LINE_PATTERN_RGB (0x0 << 16)
#define LCDIF_CTRL2_ODD_LINE_PATTERN_RBG (0x1 << 16)
#define LCDIF_CTRL2_ODD_LINE_PATTERN_GBR (0x2 << 16)
#define LCDIF_CTRL2_ODD_LINE_PATTERN_GRB (0x3 << 16)
#define LCDIF_CTRL2_ODD_LINE_PATTERN_BRG (0x4 << 16)
#define LCDIF_CTRL2_ODD_LINE_PATTERN_BGR (0x5 << 16)
#define LCDIF_CTRL2_EVEN_LINE_PATTERN_MASK (0x7 << 12)
#define LCDIF_CTRL2_EVEN_LINE_PATTERN_OFFSET 12
#define LCDIF_CTRL2_EVEN_LINE_PATTERN_RGB (0x0 << 12)
#define LCDIF_CTRL2_EVEN_LINE_PATTERN_RBG (0x1 << 12)
#define LCDIF_CTRL2_EVEN_LINE_PATTERN_GBR (0x2 << 12)
#define LCDIF_CTRL2_EVEN_LINE_PATTERN_GRB (0x3 << 12)
#define LCDIF_CTRL2_EVEN_LINE_PATTERN_BRG (0x4 << 12)
#define LCDIF_CTRL2_EVEN_LINE_PATTERN_BGR (0x5 << 12)
#define LCDIF_CTRL2_READ_PACK_DIR (1 << 10)
#define LCDIF_CTRL2_READ_MODE_OUTPUT_IN_RGB_FORMAT (1 << 9)
#define LCDIF_CTRL2_READ_MODE_6_BIT_INPUT (1 << 8)
#define LCDIF_CTRL2_READ_MODE_NUM_PACKED_SUBWORDS_MASK (0x7 << 4)
#define LCDIF_CTRL2_READ_MODE_NUM_PACKED_SUBWORDS_OFFSET 4
#define LCDIF_CTRL2_INITIAL_DUMMY_READ_MASK (0x7 << 1)
#define LCDIF_CTRL2_INITIAL_DUMMY_READ_OFFSET 1

#define LCDIF_TRANSFER_COUNT_V_COUNT_MASK (0xffff << 16)
#define LCDIF_TRANSFER_COUNT_V_COUNT_OFFSET 16
#define LCDIF_TRANSFER_COUNT_H_COUNT_MASK (0xffff << 0)
#define LCDIF_TRANSFER_COUNT_H_COUNT_OFFSET 0

#define LCDIF_CUR_BUF_ADDR_MASK 0xffffffff
#define LCDIF_CUR_BUF_ADDR_OFFSET 0

#define LCDIF_NEXT_BUF_ADDR_MASK 0xffffffff
#define LCDIF_NEXT_BUF_ADDR_OFFSET 0

#define LCDIF_TIMING_CMD_HOLD_MASK (0xff << 24)
#define LCDIF_TIMING_CMD_HOLD_OFFSET 24
#define LCDIF_TIMING_CMD_SETUP_MASK (0xff << 16)
#define LCDIF_TIMING_CMD_SETUP_OFFSET 16
#define LCDIF_TIMING_DATA_HOLD_MASK (0xff << 8)
#define LCDIF_TIMING_DATA_HOLD_OFFSET 8
#define LCDIF_TIMING_DATA_SETUP_MASK (0xff << 0)
#define LCDIF_TIMING_DATA_SETUP_OFFSET 0

#define LCDIF_VDCTRL0_VSYNC_OEB (1 << 29)
#define LCDIF_VDCTRL0_ENABLE_PRESENT (1 << 28)
#define LCDIF_VDCTRL0_VSYNC_POL (1 << 27)
#define LCDIF_VDCTRL0_HSYNC_POL (1 << 26)
#define LCDIF_VDCTRL0_DOTCLK_POL (1 << 25)
#define LCDIF_VDCTRL0_ENABLE_POL (1 << 24)
#define LCDIF_VDCTRL0_VSYNC_PERIOD_UNIT (1 << 21)
#define LCDIF_VDCTRL0_VSYNC_PULSE_WIDTH_UNIT (1 << 20)
#define LCDIF_VDCTRL0_HALF_LINE (1 << 19)
#define LCDIF_VDCTRL0_HALF_LINE_MODE (1 << 18)
#define LCDIF_VDCTRL0_VSYNC_PULSE_WIDTH_MASK 0x3ffff
#define LCDIF_VDCTRL0_VSYNC_PULSE_WIDTH_OFFSET 0

#define LCDIF_VDCTRL1_VSYNC_PERIOD_MASK 0xffffffff
#define LCDIF_VDCTRL1_VSYNC_PERIOD_OFFSET 0

#define LCDIF_VDCTRL2_HSYNC_PULSE_WIDTH_MASK (0x3fff << 18)
#define LCDIF_VDCTRL2_HSYNC_PULSE_WIDTH_OFFSET 18
#define LCDIF_VDCTRL2_HSYNC_PERIOD_MASK 0x3ffff
#define LCDIF_VDCTRL2_HSYNC_PERIOD_OFFSET 0

#define LCDIF_VDCTRL3_MUX_SYNC_SIGNALS (1 << 29)
#define LCDIF_VDCTRL3_VSYNC_ONLY (1 << 28)
#define LCDIF_VDCTRL3_HORIZONTAL_WAIT_CNT_MASK (0xfff << 16)
#define LCDIF_VDCTRL3_HORIZONTAL_WAIT_CNT_OFFSET 16
#define LCDIF_VDCTRL3_VERTICAL_WAIT_CNT_MASK (0xffff << 0)
#define LCDIF_VDCTRL3_VERTICAL_WAIT_CNT_OFFSET 0

#define LCDIF_VDCTRL4_DOTCLK_DLY_SEL_MASK (0x7 << 29)
#define LCDIF_VDCTRL4_DOTCLK_DLY_SEL_OFFSET 29
#define LCDIF_VDCTRL4_SYNC_SIGNALS_ON (1 << 18)
#define LCDIF_VDCTRL4_DOTCLK_H_VALID_DATA_CNT_MASK 0x3ffff
#define LCDIF_VDCTRL4_DOTCLK_H_VALID_DATA_CNT_OFFSET 0

#ifdef CONFIG_MX6SX
extern void vadc_power_up(void);
extern void vadc_power_down(void);
extern void pcie_power_up(void);
extern void pcie_power_off(void);
#endif

/*
* If ROM fail back to USB recover mode, USBPH0_PWD will be clear to use USB
* If boot from the other mode, USB0_PWD will keep reset value
*/
#define is_boot_from_usb(void) (!(readl(USB_PHY0_BASE_ADDR) & (1<<20)))
#define disconnect_from_pc(void) writel(0x0, OTG_BASE_ADDR + 0x140)

#endif /* __ASSEMBLER__*/
#endif /* __ASM_ARCH_MX6_IMX_REGS_H__ */

Still when I burning my image it will show the DRAM size is 1G.

But there is 4G RAM on my board.

Where did I miss ?

 Thanks in Advanced!

1 回复

1,960 次查看
Yuri
NXP Employee
NXP Employee

Hello,

 Please refer to Chapter 1 (Porting U-Boot from an i.MX 6/7 Reference Board to an i.MX 6/7 Custom
Board) in “i.MX_BSP_Porting_Guide.pdf”.

  In particular, in Uboot file “include/configs/mx6 <board>.h” check / modify (if needed) parameters :
 - CONFIG_NR_DRAM_BANKS: Number of ddr banks.
 - PHYS_SDRAM_SIZE: Configure the DDR size in MB.
 - PHYS_SDRAM: Physical address for the DDR memory.

Regards,
Yuri