i.MX6: Problem on the size of the partition after a formatting in FAT32 of a SDcard

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX6: Problem on the size of the partition after a formatting in FAT32 of a SDcard

1,798件の閲覧回数
gaylordlebrun
Contributor II

Hello to all,

Here is my situation, I possess a SDcard of 8 Go, when I take up it on my system, the only partition makes approximately 7.4 Go. But after I format (mkfs.vfat -I -F 32  /dev/<>p1) this partition is no more than of 2 Go.

How may I make for preserved the initial size?

Thank you in advance for any answers.

Best regards

Gaylord

ラベル(2)
タグ(3)
0 件の賞賛
返信
3 返答(返信)

1,651件の閲覧回数
b36401
NXP Employee
NXP Employee

I do not know what goes wrong in your case. I was unable to reproduce the issue.
Please try to omit "-I -F 32" they are not actually required but maybe they causes this issue somehow.

Have a great day,
Victor

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

1,651件の閲覧回数
gaylordlebrun
Contributor II

Thanks Victor

But I try to omit "-I -F 32" and It is the same result, I have no more than 2Go of storage.

Best regards

Gaylord

0 件の賞賛
返信

1,651件の閲覧回数
yan2anfei
Contributor III

the fdisk has bug.

0 件の賞賛
返信