i.MX6 : Power-Up Sequence about VDD_HIGH_IN

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX6 : Power-Up Sequence about VDD_HIGH_IN

ソリューションへジャンプ
1,952件の閲覧回数
koichisakagami
Contributor II

Dear community,
I have a question about power-up sequence about VDD_HIGH_IN .

[Background]
In the datasheet , it is described that
VDD_SNVS_IN supply must be turned ON before any other power supply. It may be connected
(shorted) with VDD_HIGH_IN supply.

I did not see any sequence requirements on VDD_HIGH_IN.

[Question]
When VDD_SNVS_IN is connected with VDD_HIGH_IN ,
does the VDD_HIGH_IN have to  turned on before any other power supply ?

Best Regards,
Koichi Sakagami

ラベル(1)
0 件の賞賛
返信
1 解決策
1,434件の閲覧回数
SergioSolis
NXP Employee
NXP Employee

VDD_SNVS_IN has to be turned on before anything else. If VDD_HIGH_IN is connected to VDD_SNVS_IN, it will be turned on practically at the same time.

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
1,435件の閲覧回数
SergioSolis
NXP Employee
NXP Employee

VDD_SNVS_IN has to be turned on before anything else. If VDD_HIGH_IN is connected to VDD_SNVS_IN, it will be turned on practically at the same time.

0 件の賞賛
返信
1,434件の閲覧回数
satoshishimoda
Senior Contributor I

Hi SerchMX,

Could you let me know the sequence of VDD_SNVS_IN and VDD_HIGH_IN when these are not connected also?

I guess VDD_SNVS_IN -> VDD_HIGH_IN -> other supplies is correct sequence.

Is this correct?

And I guess if user don't preserve this sequence, i.MX6 cannot power up correctly and i.MX6 is damaged.

Is this correct?

Best Regards,

Satoshi Shimoda

0 件の賞賛
返信
1,434件の閲覧回数
koichisakagami
Contributor II

Dear SerchMX san,

Thank you for your answer.

I got it.

Best Regards

Koichi Sakagami

0 件の賞賛
返信