i.MX6 : Power-Up Sequence about VDD_HIGH_IN

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

i.MX6 : Power-Up Sequence about VDD_HIGH_IN

跳至解决方案
1,954 次查看
koichisakagami
Contributor II

Dear community,
I have a question about power-up sequence about VDD_HIGH_IN .

[Background]
In the datasheet , it is described that
VDD_SNVS_IN supply must be turned ON before any other power supply. It may be connected
(shorted) with VDD_HIGH_IN supply.

I did not see any sequence requirements on VDD_HIGH_IN.

[Question]
When VDD_SNVS_IN is connected with VDD_HIGH_IN ,
does the VDD_HIGH_IN have to  turned on before any other power supply ?

Best Regards,
Koichi Sakagami

标签 (1)
0 项奖励
回复
1 解答
1,436 次查看
SergioSolis
NXP Employee
NXP Employee

VDD_SNVS_IN has to be turned on before anything else. If VDD_HIGH_IN is connected to VDD_SNVS_IN, it will be turned on practically at the same time.

在原帖中查看解决方案

0 项奖励
回复
3 回复数
1,437 次查看
SergioSolis
NXP Employee
NXP Employee

VDD_SNVS_IN has to be turned on before anything else. If VDD_HIGH_IN is connected to VDD_SNVS_IN, it will be turned on practically at the same time.

0 项奖励
回复
1,436 次查看
satoshishimoda
Senior Contributor I

Hi SerchMX,

Could you let me know the sequence of VDD_SNVS_IN and VDD_HIGH_IN when these are not connected also?

I guess VDD_SNVS_IN -> VDD_HIGH_IN -> other supplies is correct sequence.

Is this correct?

And I guess if user don't preserve this sequence, i.MX6 cannot power up correctly and i.MX6 is damaged.

Is this correct?

Best Regards,

Satoshi Shimoda

0 项奖励
回复
1,436 次查看
koichisakagami
Contributor II

Dear SerchMX san,

Thank you for your answer.

I got it.

Best Regards

Koichi Sakagami

0 项奖励
回复