i.MX6 Port table

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX6 Port table

337 Views
ban45
Contributor III

Hi

Is there a list datasheet of signal names (src_bt_cfg, 6 or usdhc_data, 3, etc.) that can be assigned to each port?
This is because I want to compare the output result of config tool for i.MX v7 with the signal name. (Html_report_Pins.html)

i.MX 6ULL Applications Processors for Industrial Products Rev1.2 11/2017 does not provide detailed assignable signal names (such as src_bt_cfg, 6 or usdhc_data, 3).
 
Could you please tell me which datasheet to look at?
i.MX 6ULL Applications Processors for Industrial Products, Rev. 1.2, 11/2017 is
 

regard

0 Kudos
1 Reply

321 Views
b36401
NXP Employee
NXP Employee

In addition to the DataSheet you can refer to i.MX6ULL Reference Manual:
https://www.nxp.com/webapp/Download?colCode=IMX6ULLRM

0 Kudos