i.MX6 Plus - USB is unstable issue

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX6 Plus - USB is unstable issue

1,748件の閲覧回数
yen-polin
Contributor II

Hi ,

    We've implement i.MX6 Dual plus/Quad plus and Yocto 1.8 .

    USB port of HOST/OTG are unstable at both Dual plus and Quad plus .

    If we try to do "time dd if=/dev/sda1 of=/dev/null bs=8k" , then sometimes show the message as below

         ==> "usb 1-1: reset high-speed USB device number 2 using ci_hdrc" .

         ==> "Buffer I/O error on device sda1"

         ==> "usb 1-1: device firmware changed"

    So we've measure the USB signals and power , the report as attached file looks fine .

    Also we try to reduce USB trace length (under 1200mils) , but still can't fix this issue .

    So

       (1) Does it have any power rail for internal USB logic , we need to double confirm ?

       (2) Do you have any suggestion about USB Test item (EL_xx) we need to check , if we'll measure Hi-Speed USB signals again ?

       (3) Does it have any register cause these wrong message ? Could we try to disable it ?

       (4) Other recommend ?

    Thanks a lot.

Terry

ラベル(1)
2 返答(返信)

1,383件の閲覧回数
yen-polin
Contributor II

Hi ,

       I've change the value of address: 0x021b0400 to 0x14420000 from 0x514201f0 ,then it can fix this USB issue .

       Address : 21B_0400 is MMDC Core AXI Reordering Control Register .

              Thanks a lot.

1,383件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Terry

reason for instability may  be VDD_VBUS_CAP -power rail for internal USB logic,

as well as DDR errors, so recommended to test it with ddr test:

i.MX6/7 DDR Stress Test Tool V2.52

AN4589 Configuring USB on i.MX 6 Series Processors

on p.7 shows setting for improving usb signals

http://cache.nxp.com/files/32bit/doc/app_note/AN4589.pdf

Also one can check sect.3.11 USB recommendations

i.MX6 System Development User’s Guide

http://cache.freescale.com/files/32bit/doc/user_guide/IMX6DQ6SDLHDG.pdf

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------