i.MX6 Platform SDK in windows

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX6 Platform SDK in windows

1,352 Views
shamiksaha
Contributor II

Hi all,

I have very less exposure to Linux platform, and thus was hoping to use Platform SDK v1.1 for using i.MX6Q.

Can anybody suggest ways so that I can use Eclipse-based IDE on windows to run applications on Sabre-SD board, like how to build a basic app to print hello world in Serial port.

Any help would be appreciated. Thanks!!

Regards,

Shamik

Labels (1)
0 Kudos
Reply
2 Replies

1,146 Views
Yuri
NXP Employee
NXP Employee

Shamik,

  As for the Platform SDK - it is relatively easy to build it just under Linux environment.

Regards,

Yuri.

0 Kudos
Reply

1,145 Views
igorpadykov
NXP Employee
NXP Employee

Hi Shamic

one can look at attached file or SX examples with Eclipse-based IDE on windows,

it is easy to modify them for i.MX6Q

https://community.freescale.com/thread/351961

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply