Dear Support-team,
We would like to extend PCIe connection using i.MX 6 iATU.
We want to program by referring to technical documents such as specifications of iATU.
We are already referred I.MX 6 RM, patch etc to in the community.
1)Can you disclose detailed information on i.MX 6's iATU?
2)Or we could refer to document (FTF-SNT-F1121.pdf) of QorIQ (LS1).
If the IP of PCIe of i.MX 6 and QorIQ (LS1) are the same, we can refer to the attached data.
Is the IP same or not?
B.Regards,
Hi Tomohisa
1. please create service request :
https://community.freescale.com/docs/DOC-329745
2. I am afraid IP of PCIe of i.MX 6 and QorIQ (LS1) is not the same.
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------