i.MX6 PCIe exclusive access control.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX6 PCIe exclusive access control.

Jump to solution
695 Views
satoshishimoda
Senior Contributor I

Hi community,

Out partner have a question about i.MX6 PCIe controller.

They want to know whether i.MX6 PCIe controller have exclusive management.

e.g. Wait access from CPU when i.MX6 PCIe is accessing to external PCIe device.

I looked for the management function in reference manual, but I was not able to find it.

So I guess the function is not implemented in i.MX6 PCIe contoller, is this correct?

Best Regards,

Satoshi Shimoda

Labels (4)
Tags (2)
0 Kudos
1 Solution
581 Views
igorpadykov
NXP Employee
NXP Employee

Hi Satoshi

you are right, there is no special management function from

core in regard to PCIe module. CPU just can access PCIe registers

through NIC301 arbiter as shown in Figure 45-1. NIC-301 Bus System

IMX6DQRM

Best regards

igor
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
582 Views
igorpadykov
NXP Employee
NXP Employee

Hi Satoshi

you are right, there is no special management function from

core in regard to PCIe module. CPU just can access PCIe registers

through NIC301 arbiter as shown in Figure 45-1. NIC-301 Bus System

IMX6DQRM

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos