i.MX6 PCIe exclusive access control.

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

i.MX6 PCIe exclusive access control.

跳至解决方案
681 次查看
satoshishimoda
Senior Contributor I

Hi community,

Out partner have a question about i.MX6 PCIe controller.

They want to know whether i.MX6 PCIe controller have exclusive management.

e.g. Wait access from CPU when i.MX6 PCIe is accessing to external PCIe device.

I looked for the management function in reference manual, but I was not able to find it.

So I guess the function is not implemented in i.MX6 PCIe contoller, is this correct?

Best Regards,

Satoshi Shimoda

标签 (4)
标记 (2)
0 项奖励
1 解答
567 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Satoshi

you are right, there is no special management function from

core in regard to PCIe module. CPU just can access PCIe registers

through NIC301 arbiter as shown in Figure 45-1. NIC-301 Bus System

IMX6DQRM

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
1 回复
568 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Satoshi

you are right, there is no special management function from

core in regard to PCIe module. CPU just can access PCIe registers

through NIC301 arbiter as shown in Figure 45-1. NIC-301 Bus System

IMX6DQRM

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励