Hi community,
I want to confirm the connection of i.MX6 PCIe interface.
Please see the foot note of Table 2-21 in i.MX6 Hardware Development Guide (IMX6DQ6SDLHDG Rev.1).
It says "These supplies must remain powered if boundary scan test needs to be done".
Then, how about in a case that JTAG debugger is used even though JTAG boundary scan is not used?
Should I remain these supplies? or can I pull them down to GND?
Best Regards,
Satoshi Shimoda