i.MX6 PCIe can't detect issue.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX6 PCIe can't detect issue.

ソリューションへジャンプ
2,649件の閲覧回数
edwinrose
Contributor I

Hi experts,

I meet a question about PCIE bus on i.MX6.

1. When I inserted Intel EXPI9301CTBLK PCI-Express(x1) Network Adapter in my board, it can works.

2. Insert Realtek RTL8111E PCIE LAN card, the system can't detect this device, following is the console message.

2014-7-2 下午 05-19-36.jpg

Could you help us to see what is the problem for this issue?

BSP version: imx_3.0.35_4.1.0

Thanks for your help.

ラベル(2)
タグ(1)
0 件の賞賛
返信
1 解決策
1,760件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi edwin

please try solutions given in link below

mx6 + rtl8111e driver

Best regards

chip

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
1,761件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi edwin

please try solutions given in link below

mx6 + rtl8111e driver

Best regards

chip

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信
1,760件の閲覧回数
edwinrose
Contributor I

I have solved this issue, thanks for your help.

0 件の賞賛
返信