Hi community!
I'm new to this development board. MCIMX6Q-SDB
I used MFGTool2 which is downloaded from the website to download linux image L3.0.35_4.1.0_130816_images_MX6.gz
I followed this install guide
http://www.freescale.com/files/training_pdf/WBNR_LA13_IMX6QPR_PDF.pdf?lang_cd=en
when I reached page 33. I use HDMI instead of LVDS. But there is no booting process showing up.
I'm wondering why. I repeat whole processes several time, which result the same.
Changes I made comparing to the install guide
* I cannot find "12_09_01_oneiric.tgz". I use downloaded ubuntu image oneiric.gz instead. And I change the name to oneiric.tgz
* I changed ucl2.xml file accordingly
I can see the installing log from the hyper Terminal.
anyone can help?
Thanks a lot
已解决! 转到解答。
Perhaps it makes sense using the recent (Yocto) Linux BSP for i.MX6, where
some issues should be fixed (in particular, HDMI-to-DVI converter cannot be used)
Also, please check kernel command line, for example :
console=ttymxc0,115200 root=/dev/mmcblk0p2 rootwait rw video=mxcfb0:dev=hdmi,1920x1080M@60,if=RGB24 fbmem=128M vmalloc=256M
Have a great day,
Yuri
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Perhaps it makes sense using the recent (Yocto) Linux BSP for i.MX6, where
some issues should be fixed (in particular, HDMI-to-DVI converter cannot be used)
Also, please check kernel command line, for example :
console=ttymxc0,115200 root=/dev/mmcblk0p2 rootwait rw video=mxcfb0:dev=hdmi,1920x1080M@60,if=RGB24 fbmem=128M vmalloc=256M
Have a great day,
Yuri
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------