i.MX6 - MPEG2/4 transport stream display at 1920x1080

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX6 - MPEG2/4 transport stream display at 1920x1080

2,252 Views
paulschoenke
Contributor III

Hello Community!

I am looking to build a small, low cost, embedded computer that is capable of decoding and displaying MPEG-2/4 transport streams at resolutions up to 1920 x 1080. 

I am considering the Freescale i.MX6 and it looks good with exception of the transport steam input. 


Does anyone know if there is a way to convert the transport stream to bring it in through a different interface, like the camera interface or other?

We may still have the option of using a USB bridge but would prefer not to deal with the latency and restrictions of converting a video stream to USB.


Any feedback or input is welcomed and appreciated!

Thank you!

Paul

Labels (4)
0 Kudos
Reply
2 Replies

1,256 Views
igorpadykov
NXP Employee
NXP Employee

Hi Paul

I think gstreamer below links answer that

Does i.MX 6 series multimedia package provide MPEG-2 TS muxer plugin?

GStreamer crashing on i.MX6 (Boundary Devices Nitrogen6x)

L3.0.35_4.1.0_LINUX_MMDOCS

i.MX 6Quad, i.MX 6Dual, i.MX 6DualLite, i.MX 6Solo and i.MX 6Sololite Linux Multimedia Codecs Documentation.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

1,256 Views
saurabh206
Senior Contributor III

Hi,

Paul

imx6 is capable of decoding MPEG-2/4 up to 1080p.

You can connect tuner with imx6.

Saurabh

0 Kudos
Reply