Hi,
in my application I'm using an i.MX6-quad.
I measure the die temperature by:
cat/sys/class/thermal/thermal_zone0/temp.
What is the upper limit I should consider for this value so that the product
works in a safe condition?
Thanks in advance.
Best Regards,
Diego
Solved! Go to Solution.
The maximum die temperature is sepcified as the 'Junction Temperature' parameter in the corresponding part's Data Sheet document.
Have a great day,
Artur
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
The datasheet is located here:
http://www.nxp.com/files/32bit/doc/data_sheet/IMX6DQCEC.pdf
you can check table 4.1.3
The maximum die temperature is sepcified as the 'Junction Temperature' parameter in the corresponding part's Data Sheet document.
Have a great day,
Artur
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------