i.MX6 MAX die temperature

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX6 MAX die temperature

Jump to solution
1,595 Views
diegoferraiuolo
Contributor I

Hi,

in my application I'm using  an i.MX6-quad.

I measure the die temperature by:

cat/sys/class/thermal/thermal_zone0/temp.

What is the upper limit I should consider for this value  so that the product

works in a safe condition?

Thanks in advance.

Best Regards,

Diego

Labels (1)
0 Kudos
1 Solution
867 Views
art
NXP Employee
NXP Employee

The maximum die temperature is sepcified as the 'Junction Temperature' parameter in the corresponding part's Data Sheet document.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
2 Replies
867 Views
SergioSolis
NXP Employee
NXP Employee

The datasheet is located here:

http://www.nxp.com/files/32bit/doc/data_sheet/IMX6DQCEC.pdf

you can check table 4.1.3

0 Kudos
868 Views
art
NXP Employee
NXP Employee

The maximum die temperature is sepcified as the 'Junction Temperature' parameter in the corresponding part's Data Sheet document.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos