i.MX6 - Linux support for Rapid Spanning Tree Protocol?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX6 - Linux support for Rapid Spanning Tree Protocol?

2,015 Views
davidriness
Contributor I

Hello -

I am trying to find out if the ethernet driver in the Linux/Yocto build includes support for RSTP (Rapid Spanning Tree Protocol).

If so, can you point me to documentation?

All I can find is reference to Marvell saying it is supported....

Thanks in advance!

Labels (3)
0 Kudos
Reply
2 Replies

1,709 Views
b36401
NXP Employee
NXP Employee

You can refer to section 3.9 "RTSP streaming playback"

of i.MX 6 Series Yocto Project Multimedia User's Guide.

You can get the document from this pack:

http://www.freescale.com/webapp/Download?colCode=L3.10.17_1.0.0_LINUX_DOCS&Parent_nodeId=13376994810...

Have a great day,

Victor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

1,709 Views
phdm
Contributor III

Question was about RSTP (which stands for Rapid STP (which stands for Spanning Tree Protocol)), not about RTSP (which stands for Real Time Streaming Protocol).  Maybe time to switch to 5-letters acronym :smileyhappy: