i.MX6 - Linux support for Rapid Spanning Tree Protocol?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX6 - Linux support for Rapid Spanning Tree Protocol?

1,694件の閲覧回数
davidriness
Contributor I

Hello -

I am trying to find out if the ethernet driver in the Linux/Yocto build includes support for RSTP (Rapid Spanning Tree Protocol).

If so, can you point me to documentation?

All I can find is reference to Marvell saying it is supported....

Thanks in advance!

ラベル(3)
0 件の賞賛
返信
2 返答(返信)

1,388件の閲覧回数
b36401
NXP Employee
NXP Employee

You can refer to section 3.9 "RTSP streaming playback"

of i.MX 6 Series Yocto Project Multimedia User's Guide.

You can get the document from this pack:

http://www.freescale.com/webapp/Download?colCode=L3.10.17_1.0.0_LINUX_DOCS&Parent_nodeId=13376994810...

Have a great day,

Victor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

1,388件の閲覧回数
phdm
Contributor III

Question was about RSTP (which stands for Rapid STP (which stands for Spanning Tree Protocol)), not about RTSP (which stands for Real Time Streaming Protocol).  Maybe time to switch to 5-letters acronym :smileyhappy: